The PAC Config Tool allows users to connect to the Xpress shell to do the online development of the HMI project. It also allows users to upload the project from the PAC to the PC (Get). It also allows users to download the project from the PC to the PAC (Send).
Note the resolutions for the PAC Xpress is different than the XPR2 panels and thus a project from an XPR2 could not be downloaded to a PAC.
Port 81 allows connecting to the PAC Config Tool.
Users can connect to the Xpress through an internet browser by using the PAC's ip address.
Similar to powering on an XPR2 panel, this will launch the Xpress shell. From there, Run can be used to launch the HMI project:
Or Disconnect and then Design to edit the HMI project.

2/15jh
1NOV18 JD