Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Software - Assigning Limit and Home Inputs (HLBIT)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Software - Assigning Limit and Home Inputs (HLBIT)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
IPA Software - Assigning Limit and Home Inputs (HLBIT)

Print Friendly and PDF
Products: IPAxx-HC
 
The initial release of IPA drive/controller firmware 4.40 adds new functionality to the HLBIT command that assigns limit and home inputs.
This extension was added to ACR9xxx firmware in firmware version 1.41 (2.41 for 9600).

The original implementation of HLBIT is still supported for backwards compatibility.
example : HLBIT X3   or AXIS0 HLBIT 3
Input 3 is the positive limit, Input 4 is negative limit, Input 5 is home. 
The user was only allowed to designate the positive limit, the next two consecutive bits were automatically assigned as negative limit and home. 

NEW
HLBIT X(1,3,5) sets positive, negative, and home bits in that order. If any bits are out of range, the whole command is rejected. The second and third numbers are optional resulting in automatic assignment of next bit.
HLBIT X(1) sets positive, negative, and home bits to 1, 2, 3 respectively.
HLBIT X(1,3) sets positive, negative, and home bits to 1,3,4 respectively.

Status Parameters 

P12420 still displays positive limit bit number
P12437, P12438, P12439 display positive, negative and home bit numbers respectively. 
(Note these are read-only parameters.)

Home to Limit
This new syntax also allows homing to a limit.  If the home limit is the same as an end of travel limit, then the controller will home to that limit when the JOG HOME command is issued.  

There are two differences from standard homing to prevent moving beyond end of travel limit.
1. If Home backup is enabled and home is also an end of travel limit, the user's choice of active edge is ignored. Instead the active edge will always the inside edge, the same edge that causes hard limit deceleration. 
For the positive limit, this is the negative edge, for the negative limit, this is the positive edge.
2. When the combined home/EOT limit is hit, the hard limit deceleration value will be used instead of the jog deceleration.
The user's choice of final direction and final approach speed are still used.