Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Software - Torque Enable Inputs Functionality
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Software - Torque Enable Inputs Functionality
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
IPA Software - Torque Enable Inputs Functionality

Print Friendly and PDF

The IPA provides dual Torque Enable channels as a means of preventing the drive from delivering rotational force to its connected electric motor or linear force for a linear motor. To ensure a high degree of safety, two independent Torque Enable control channels are implemented in hardware. The Torque Enable circuit in the IPA is designed such that a fault in one control channel will not affect the other channel's ability to prevent the drive from starting, i.e. the Torque Enable function of the IPA drive is tolerant to any single fault. It may not be tolerant to an accumulation of faults. If one or both Torque Enable control inputs requests the torque to be disabled, the drive will not start, even if the drive's software malfunctions and tries to cause the motor to turn.

The Torque Enable function is implemented in hardware and overrides all software activities. The only software involvement is to report torque status to the user via error and fault bits.

The Torque Enable terminals are on the Auxiliary connector on the top of the IPA (x7 connector).

The IPA ships with jumpers (22AWG solid) so that with no additional connections, users may enable the IPA from the user programs or within ACR-View's configuration Wizard during setup.

These jumpers connect the TRQ_EN_24V to the TRQ_EN1 and TRQ_EN2 and the commons together. (This is limited to 30mA so this is only designed for these jumpers.)

These are redundant inputs and should both be set or cleared within 1.6seconds of each other. From this, the IPA can be software enabled. 

If the inputs stay opposite longer than 3 seconds, the drive faults and requires cycle power (or REBOOT from ACR-View) and cannot be software enabled.

State Diagram showing operation:

The torque enable status are shown in ACR-View's Common Status Panel.

The bits for these are 10009 Torque Enable Fault;  10010 Torque Enable Open;  10011 Torque Enable Health Event.

For the drive enabled:

 

The torque enable status are shown in ACR-View's Common Status Panel. For the torque enable inputs open:

The torque enable status are shown in ACR-View's Common Status Panel. For the torque enable inputs opposite:

keywords:

status state machine

2/15jh

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply