Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Parker MotionSizer - Temperature Rise Calculation
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Parker MotionSizer - Temperature Rise Calculation
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
  • AC/DC Industrial Drives+
  • Gearheads+
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners-
    • IForce Linear Servo Motors & Positioners-
      • When should I used a linear motor stage?
      • What are the main precision application types for linear motor stages?
      • Can Parker provide custom linear motor stage solutions?
      • 110 WD0 Motor Specifications
      • 310 Coil Bar Side Mounting Locations
      • Air Cooling and Liquid Cooling Notes
      • Can I use the motor in vertical applications?
      • Current Derate for less <0.5pitch moves
      • D Dual parallel winding specs
      • Different types of linear motors
      • Do the magnets lose their magnetism with time?
      • Does the motor coil float between the magnets?
      • Hall-Effect, Home and Limit Module Wiring
      • High Pot Option
      • How do I select a linear motor?
      • How to Wire MHED Limit/Home/Halls Module
      • IForce Coil Compatibility in Vacuum Environments
      • Importance of mechanical alignment
      • Inspection Report
      • LEM Feedback Troubleshooting & Replacements
      • LME vs PLME Linear Magnetic Encoders
      • ML18 Track Weights
      • Motors used underwater or in the presence of oils
      • No motors listed in WinTips motor database?
      • Old IForce actuator part numbering
      • Omega 44004 Thermistor Info
      • Parker MotionSizer - Temperature Rise Calculation
      • Phasing Diagram
      • Renishaw Optical Encoders
      • Trilogy Electrical Pitches
      • Trilogy Extension Cables
      • Trilogy High Flex Cable Specifications
      • Trilogy IForce Cooling Options
      • Trilogy IForce Custom High Vacuum Options
      • Trilogy Motor Summary & Drive Compatibility
      • Trilogy Motors with Non-Parker Servo Drives
      • What are the minimum bend radii of Trilogy THF flex cables?
      • What voltage for IForce hall-effect sensors?
      • Which MHED is used within the positioners?
      • Why do some motors have steel laminations?
      • Why lamination designs skew or angle their magnets
      • Winding Tolerances and Resistance Measurement
    • MX80+
    • mSR+
    • Ripped Series Linear Motors & Positioners+
    • LXR+
    • mPR+
    • XE+
    • XR+
    • ZP Wedge+
    • P8S Position Sensor order codes
    • How can I know if a given actuator is suitable for use in a specific environment?
    • Manufacturer Grease Standardization
    • I need speed and accuracy over a long length. What type of actuator should I use?
    • What type of encoder options are available for the Trilogy Series?
    • What type of material is used for the base of the Trilogy Linear Motor Positioners?
    • LBB / LBZ / LBN Linear Actuator Model Numbers
    • Parker Limit and Home Sensor Compatibility
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
Parker MotionSizer - Temperature Rise Calculation

Print Friendly and PDF
Even though Parker MotionSizer does not have the coil temperature rise calculation like WinTips, this is a fairly straight-forward calculation.

This spreadsheet calculates the temperature rise based upon the continuous force required for the application.

As an example, presume an application in MotionSizer is generated and the R10-3S is selected. The continuous force required for this application 191.05 lbf. In MotionSizer this is the Motor Rated Force on the Motor Selection screen. If you have a list of motor/drive combinations make sure you highlight that motor/drive combination by clicking on that row. Then the Motor Rated Force above shows the continuous force.

The first column shows the calculations with the parameters. The second column with the R10-3 has Excel cell referenced in the formulas allowing easier expansion or copy & pasting for evaluating multiple coils.

Simple Sizing Spreadsheet


For the experienced users that know WinTIPS and still want to know the thermal rise temperature, alternatively this temp_calculator that has all the Trilogy motors, just input the continuous force required (shown in the Motor Selection screen in Parker MotionSizer) for the application and the ambient temperature:

Temperature Calculator - All Trilogy Motors

If the force is too far beyond what the motor can do, the calculation isn't relevant and it'll change to ###### (like WinTIPS does).
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply