In C3 ServoManager, Optimization window with release 9-0 and higher, the object tree can be activated. This has all objects within the Compax3 in a format similar to the Status Values, sorted by object number. From here, objects can be clicked and dragged to the Status Display or graphed using the Oscilloscope.
To activate the object tree, use the menu that's in the bottom center of the screen: