Go to Parker.com
Search
Sign in
Technologies
Aerospace
Climate Control
Electromechanical Group
Filtration
Fluid and Gas Handling
Hydraulics
IoT
Pneumatics
Process Control
Sealing and Shielding
Other Groups
Parker Indego
Blogs
Forums
Knowledge Bases
Parker Community
Technologies
Aerospace
Climate Control
Electromechanical Group
Filtration
Fluid and Gas Handling
Hydraulics
IoT
Pneumatics
Process Control
Sealing and Shielding
Other Groups
Parker Indego
Blogs
Forums
Knowledge Bases
Search
User
Site
Search
User
Home
Technologies
Electromechanical Group
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base
Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
Technologies
Electromechanical Group
Electromechanical - Industrial
More
Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base
Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
Electromechanical – Industrial Support Forum
Electromechanical Industrial Knowledge Base
Members
Sub Groups
More
Cancel
New
Electromechanical - Industrial requires membership for participation - click to join
Electromechanical Knowledge Base & Frequently Asked Questions
-
Motion and Machine Controllers
+
ACR Controllers
+
PAC120
+
PAC340
-
PAC320 (Discontinued)
+
3rd Party Samples
+
Embedded Xpress
+
Errors
+
Hardware
+
PAM IDE
+
Programming Tips
+
Web Visualization
Quick Start and Online Training Videos
Adding New Devices
Auto Addressing enabled by default
Cam and Gear Program Sample & Video
Common PACIO Troubleshooting Tips
Compax3 Linear servo motor settings with PAC
Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
Reading G Code from a file to develop a CNC machine
Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
FTP support
How can I send ASCII strings to or from the PAC?
How do I configure and gear to the PACIO-454-01 Module?
How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
How do I use variables in G code?
How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
How to Set and Get Time / Date / Time Zone Pre-1.4
How to Update Devices and their Descriptor files
How to Update PAC project without Parker Automation Manager software?
How to Update a PAC Firmware? Flashback instructions
How to Upload a Program?
How to Use the InteractX OPC Quick Client with the PAC
How to set up EtherNet/IP Communications with an Allen Bradley PLC
How to set Scaling for Parker Mechanics
How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
IO settings for EtherCAT_Master: How to see IO update while in Stop
Log Data to a File
Minimum Internet Explorer version for Xpress and Visualization options
PAC CNC & Multi-Axis Capabilities, Samples & Video demos
PAC CNC visualization
PAC System Time Access and Edits
PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
PAC with .Net or LabView or InteractX: Using OPC DA Server
PAC with Modbus: What addresses for tags?
Reading Torque from Pseries drive
Remanent Variables: Retain vs Persistent Retain
Retentive Memory details
SDO Read / Write PAC to/from Compax3 I31
SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
Sample Continuous Function Chart CFC Program: time based counter
Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
Sample Ladder Logic LD Program: Time based counter
Sample SFC Program: time based counter
Sample Stuctured Text ST Program: Time Based Counter
Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
Single Axis Sample Program with Visualization
Two Axis Sample Program with Visualization
Using the PAC as a Modbus TCP Master Device
Using the PAC as a Modbus TCP Slave Device
VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
Video: Parker's PAC, the Automation Controller Based on IEC61131-3
What's the 16# in the axis scaling default of 16#10000?
Working with recipes in the PAC
Does the PAC have a first scan flag?
Error when switching Active Application
Using tappets during cam motion
WebVisualization not working in PAC terminal (PTA)
Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
Does PAC act as a OPC-UA server or client, or both?
How do I upgrade the PAC from OPC-DA to OPC-UA?
How do I use OPC-UA with the PAC?
PACIO-441-01 analog current input module
Sample code for PACIO-442-02 and PACIO-441-02 analog modules
What ports get used with PAC Ethernet connections?
C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
CSV Reader Library for the PAC
Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
eCL Homing notes with PAC via EtherCAT
EtherCAT communication between the PAC and AC30 drive
How to add images to a visualization in WebVis
How to reset the EtherCAT bus
Parker Tap Adapter for EoE communications
User Management in the Parker Automation Controller
Using MC_TouchProbe with Compax3 Series Drives
Using MC_TouchProbe with P Series Drives
Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
+
6K (Discontinued)
+
General Technology Information
+
Virtual Engineer
+
Visualization and Human Machine Interface (HMI)
+
Servo Drives and Servo Drive/Controllers
+
Stepper Drives and Stepper Drive/Controller
+
Gearheads
+
AC and DC Drives and Inverters
+
Servo Motors
+
Step Motors
+
Linear and Rotary Positioners
+
Electric Cylinders
+
T-Slot Aluminum Framing
+
C3 + Xpress + ETH
How can I stay updated on Parker electromechanical and drives product news?
+
Legacy (Discontinued)
+
Other
Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
What replaces the Gemini GV6K servo drive controller?
Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
Revision
Creation Date
Revision Author
Select All
Current Revision
31 Oct 2018 11:38 PM
Jack DeGrano
2
Revision #2
20 Feb 2018 3:26 AM
Former Member
1
Revision #1
1 Oct 2017 9:45 AM
Electromechanical and Drives Team
Compare Versions
View current version