Users may add External Files of any sort to a project, storing these onto the SD card of the PAC. These may include drawings, presentations, user manuals, etc.
Right-click on the project in the POUs (or Application in the Devices) and select External File...

This will open the Add External File window:

Select the file path and whether to embed or to link to it or both:

The file now appears:

1/15jh