Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Sample Continuous Function Chart CFC Program: time based counter
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Sample Continuous Function Chart CFC Program: time based counter
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
  • -Motion and Machine Controllers
    • +ACR Controllers
    • +PAC120
    • +PAC340
    • -PAC320 (Discontinued)
      • +3rd Party Samples
      • +Embedded Xpress
      • +Errors
      • +Hardware
      • +PAM IDE
      • +Programming Tips
      • +Web Visualization
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Sample CFC Program: time based counter

Here's a simple sample Continuous Flow Chart CFC program. It starts when the PLC application starts and increments a counter variable every second.

PAC_Counter_CFC.zip

Note the PLCcounter variable should be added to the Global Variable List in your program. You can set this as a DINT. With it in the GVL, this will be available to other programs in the application.


For how to import, see this FAQ:
Programming Tip: Save Time by reusing Code (Export / Import Programs & Function Blocks)

Here's a video it running within PAC IDE software:


Note a PAC320 hardware controller isn't necessary to run this. You can use an application with a CODESYS Control Win V3. Under Online > Simulation. Then you can after Build (F11), click Online >Login. This will create a virtual PLC and allow you to run PLC simulation (Play or F5). Here's a screen capture and project archive:

CFC_Counter_PCsimulation_projectarchive.zip


1/15JH