Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project

Print Friendly and PDF

The symptom of the problem is, if you load a project and click on the Design button,

the designer starts to load then pauses and pops up a message referring to an Error Step 3.

The issue is that the Adobe Flash security port 843 is being blocked due to another program using it.

The program that is most likely causing the problem is DropBox.

DropBox is using a port that is used by and generally recognized to be assigned to Adobe Flash. There is a proxy server setting in DropBox if left blank or default, DropBox uses and conflicts with port 843 that Flash uses.

You can shut down DropBox for the period you are using PFD Manager which frees up port 843 and clears the conflict.

Close DropBox then Close PFD Manager completely. Then Open PFD Manager and the error will not appear as long as DropBox is not running.

added 3/2/15 dm

keyword: Step3, "Step 3", Step 2, "Step 2"

keyword added 8/29/16jh

  • Xpress
  • Step
  • XPR
  • Dropbox
  • XT
  • PFD
  • Port 843
  • Firewall
  • Proxy
  • XPR2