Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
IPA Software - Change Direction of Travel (What is Positive/Negative Motion)

Print Friendly and PDF

In some applications it may be desirable or necessary to change the controllers sense of positive and negative direction for an axis. The following methods will change both the commanded direction and encoder direction for an axis.

Set the Invert Motion Direction Flag bit 8455. Requires ESAVE command to retain setting after power cycle from terminal window, or save programs checked when within a program.

SET BIT 8455

Notes:

  • The Invert Motion Direction Flag is not part of the configuration wizard but could be added to the Defines or a PBOOT program that initializes application settings.
  • SET or CLR of the Invert Motion flag is only allowed while the Drive is off/disabled for the axis. NOT VALID WHILE DRIVE ENABLED error will result if SET or CLR is issued while the drive is enabled. If the error occurs in a running program, that program will HALT automatically.
  • These commands do not change the assignment of positive and negative home sensors, so these may need to be rewired, or re-assigned with the HLBIT command.

    ie, If HLBIT X 0, this would be positive limited switch is input0, negative limit is input1 and home sensor is input2. To reverse, HLBIT X (1,0,2) would switch the limits. This can't be done in the configuration wizard but can be done via the terminal emulator or within the program.


    INVERTING SECONDARY ENCODER INPUT

    For applications using the secondary encoder input, its direction can be changed with the MULT command.

    P00>AXIS0 DRIVE OFF X

    P00>ENC1 MULT
    4

    Change the sign of the encoder multiplier:

    P00>ENC1 MULT-4
    Issue ESAVE to retain these value after power cycle.

    Notes:

    • Default positive motor direction is clockwise looking at the motor shaft (or for linear motors, away from the cable exit).
    • ENC MULT for the motor feedback will work but in querying will always respond as 4. Thus not recommended, use SET 8455.
    • For non-Parker motors where the encoder direction is needed to be inverted, use C20, Encoder Polarity (ENCPOL) parameter. This is not affected by the ENC MULT command.
    • With some drive/motor combinations, the command direction (DAC GAIN) and encoder direction (MULT) may need to be different. For Example DAC0 GAIN 3276.8 and ENC0 MULT-4. Use caution when making this type of change as it could result in a runaway condition.
    3/15jh
    • Share
    • History
    • More
    • Cancel
    • Sign in to reply