Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Software - INTCAP (Position Capture)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Software - INTCAP (Position Capture)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
IPA Software - INTCAP (Position Capture)

Print Friendly and PDF

Products: IPA

The IPA has two Capture Registers and can performance high speed captures on both the primary/motor encoder  (ENC0) and the aux/secondary encoder (ENC1). The table below defines what inputs can trigger the captures. Mode is used by the INTCAP, MSEEK, HSINT, CAM ON TRG and GEAR ON TRG commands to tells the controller which input is triggering the capture. 

Capture Register: Specifies which register is armed to hold the captured position.
If the hardware capture register is not specified, the hardware capture register index is the same as the feedback encoder index of the axis used to enable the hardware capture. The capture complete flag and hardware capture parameter for the encoder capture is selected based on the axis used to enable the hardware capture.

In this example, ENC0 (primary feedback) is attached to AXIS0, therefore the default Capture Register is 0
INTCAP X0 
REM Mode 0 = rising Z marker
INTCAP X1 
REM Mode 1 = falling Z marker
INTCAP X6
REM Mode 6  = falling edge Input
AXIS0 INTCAP 2
REM Mode2 = rising edge of Inp 5
REM Hardware Capture Parameter -- P12292
REM Capture Complete Flag -- BIT777

If the hardware capture register is specified then the capture parameter must also be specified. The capture complete flags and hardware capture parameters are still in pairs, but are not based on the axis used to enable the hardware capture.
AXIS0 INTCAP 11 CAP1 P12548
REM Mode 11-- Inp 4
REM Hardware Capture Parameter -- P12548
REM Capture Complete Flag -- BIT809
 
The only valid way to capture the second encoder is using input 4. The other 2 high speed inputs 5 and 6 are used as the encoder so cannot be used to also capture. 

The INTCAP command is axis/encoder specific, so we need to relate the axis to an encoder. By default in the IPA  ENC1  (secondary encoder)is attached to the AXIS1 (phantom axis). Because of this we can directly address the INTCAP command without additional set-up.

the two valid modes are :

11  : rising edge of Input 4
15  : falling edge of input 4

code would look like this

AXIS1 INTCAP 11   : rem rising edge of input 4
or
AXIS1 INTCAP15  : rem falling edge of input 4
Or 
AXIS1 INTCAP10 CAP0 P12292  : rem rising edge of input 4
or 
AXIS1 INTCAP14 CAP0 P12292  : rem falling edge of input 4

Table Key
MRK= Encoder Z Mark
INP=Digital Input
+ = Rising Edge
- = Falling Edge
ENC0 ENC0 ENC1 ENC1
CAP0 CAP1 CAP0 CAP1
Mode
0 +MRK 0
1
2 +INP 5 +INP 6
3 +INP 6 +INP 5
4 -MRK 0
5
6 -INP 5 -INP6
7 -INP 6 -INP 5
8
9
10 +INP 4 +INP 4
11 +INP 4 +INP 4
12
13
14 -INP 4 -INP 4
15 -INP 4 -INP 4

 

 

jw 19-MAR-2015

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply