Here's a simple sample Structured Text ST program. It starts when the PLC application starts. It enables the motor (MC_Power), homes the axis (MC_Home), and then extends and retracts repeatedly with a time delay after each move.
Select the project that matches your version of Parker Automation Manager:
PAM1.4: Motion_ST_PAM1.4
PAM1.2: Motion_ST_PAM1.2
Here's a video of it running within the PAC IDE software: MOBILE USERS CLICK HERE
Note: A PAC320 hardware controller isn't necessary to run this. See below for details:
For PAM1.4:
Under the "Online" tab at the top of the PAM window, make sure "Simulation" is checked. Whenever you go to login now, PAM will run a simulated device to run your project.
Make sure to uncheck this box when you want to connect and login to a physical PAC.
For PAM1.4:
Under the "Online" tab at the top of the PAM window, make sure "Simulation" is checked. Whenever you go to login now, PAM will run a simulated device to run your project.
Make sure to uncheck this box when you want to connect and login to a physical PAC.
For PAM1.3 or earlier:
You can use an application with a CODESYS Control Win V3 device (You must add this). Under Online > Simulation. Then you can after Build (F11), click Online > Login.
This will create a virtual PLC and allow you to run PLC simulation (Play or F5). Here's some screen captures:


Note, if you are using CODESYS SoftMotion Win V3 it will launch a DOS window allowing simulation of motion and will run for two hours before disabling. This window can be minimized but motion simulation is disabled when this window is closed.

3/15jh
1NOV18 JD