Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Misc - Absolute Encoder Compatibility (EnDat)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Misc - Absolute Encoder Compatibility (EnDat)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
IPA Misc - Absolute Encoder Compatibility (EnDat)

Print Friendly and PDF

An absolute encoder is a rotary feedback device that retains position information even when powered off. Its main use is to eliminate the need to "home" the axis when powered on. They can be divided into two kinds: single-turn and multi-turn. Single-turn absolute encoders, like normal (incremental) encoders, can still measure long distances (typically millions of revolutions). The difference is that single-turn absolute encoders retain their orientation when turned off, and multi-turn absolute encoders retain their orientation AND the number of revolutions they have gone.

There are many types of absolute position feedback devices. Sine-Cosine ("SinCos") encoders are one very common technology. Within this branch of absolute encoders, two appear on Parker motors. These are the Heidenhain EnDat and the Stegmann Hiperface.

The Heidenhain EnDat is an option on MPP/MPJ motors. It is compatible with the Aries servo drive and the Compax3 with the F12 feedback option.

The Stegmann Hyperface is available on the SMN and MPP/MPJ motors. These encoders are compatible with the Compax3 drive with F11 feedback option.


Heidenhain model numbers are EQI-1331 (multiturn 8D is p/n 811814-08), ECI 1317 (9D single-turn) and EQI 1329 (6D multi-turn) and EQI 1331 (7D multi-turn).

The 8D can be run in pure digital mode EnDat 2.2 but also has the analog commutation track for backwards compatibility as a 7D replacement (EnDat 2.1).

SICK (Stegmann) part numbers are SRS50 (single-turn) and SRM50 (multi-turn).

SM and BE motors are available as custom with absolute encoders. Note for applications only needing higher resolution there is the -L encoder (5000 lines = 20,000 counts/rev post quadrature resolution) which is a standard incremental encoder. The above absolute encoders are physically too large to fit inside the back of the 23 frame servo motors; but we can provide the Heidenhain EQI1130 within a SM23 and BE23. We've done so already on numerous custom requests. The EQI1130 encoder is EnDat 2.1 and is 18 bit resolution (262,144 counts per revolution), multiturn with 4096 revs.

Encoder Turns Resolution IPA Cable Aries Cable Compax3 Cable
Heidenhain EnDat 8D Multi 19bits (524,288 ppu), 4096 turns IPAxx-HC F-1A2-xx AR-xxAE, AR-xxPE, AR-xxCE F-1A2-xx F12 option F-2A2-xx
Heidenhain EnDat 7D* Multi 19bits (524,288 ppu), 4096 turns IPAxx-HC F-1A2-xx AR-xxAE, AR-xxPE, AR-xxCE F-1A2-xx F12 option F-2A2-xx
Heidenhain EnDat 9D Single 17bits (131,072 ppu) IPAxx-HC F-1A1-xx AR-xxAE, AR-xxPE, AR-xxCE F-1A1-xx F12 option F-2A2-xx
Heidenhain EnDat 6D** Multi 17bits (131,072 ppu), 4096 turns Not compatible  N/A Not compatible N/A F11 option F-2B1-xx
Stegmann Hyperface 6S Multi 16bit (65,536 ppu), 4096 turns Not compatible  N/A Not compatible N/A F11 option F-2B1-xx
Stegmann Hyperface 9S Single 16bit (65,536 ppu) Not compatible N/A Not compatible N/A F11 option F-2B1-xx
Stegmann Hyperface 5D (SMN motors) Multi 16bit (65,536 ppu), 4096 turns Not compatible N/A Not compatible N/A F11 option F-2B1-xx

 

The IPA now also has support for Biss-B /  BiSS-C and Hyperface DSL. Available now as custom motors (contact your local Parker ATC for price quote)

See this FAQ for details on Biss support IPA MISC - ABSOLUTE ENCODER COMPATIBILITY (BISS-B AND BISS-C)

 

* The 7D is no longer offered by Heidenhain. The 8D can be used in place. It was the same resolution as the 7D and works with the Aries and Compax3 without any changes at the drive necessary.

** The 6D is no longer offered by Heidenhain. The 7D can be used in place. With the Aries drives use the command ISIN -2 to lower the feedback resolution 2bits from 19bits to 17bits for replacements.

 

3/15jh added 8D.

11/13 jh corrected 6S/9S resolution. added note on BE23/SM23.