Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range

Print Friendly and PDF

When using EnDat or BiSS-C multi-turn absolute encoders with the IPA it may be helpful to reset the zero position to better align with the system mechanics.

To reset the absolute encoder position, move the motor to the desired location.  Then, in the terminal, issue the command C62=0.
C62 can also be used to set to a non-zero position if that is more useful in your application.  C62=12345 sets its current absolute position to 12345.
Beginning with firmware version 4.41, the user can also selected the range of the absolute position:
(assuming the standard multi-turn resolution of 4096)
C185=0  ......range will be  -2047   to   +2048     This is the default for backwards compatibility of previous Aries Controller applications.  Note that the Aries Controller is obsolete and is not compatible with BiSS-C encoders.
C185=1   .....range will be 0 to 4096
jw -july 2015
UPDATED 05APR2017 DC