Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX
      • InteractX Misc - Re-register older versions of Interact X (versions 1.x through 3.4) NO LONGER SUPPORTED
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
      • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
      • InteractX Misc - How to Edit Text Alt+Double-click
      • Reading and Writing Allen Bradley Logix tags that are strings
      • Serial Communications Driver error on Com1 on boot of the runtime system.
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)

Print Friendly and PDF

Symptom:  Interact X 4.0 USB Key is Plugged in but I can't access the ComServer (or its states its in Demo mode).

NOTE: The updates to make 4.1 compatible with Windows 10 includes updates to the HASP key drivers and it now uses Sentinel drivers so this FAQ only applies to earlier versions of InteractX. There could be a conflict in drivers if two different software were using HASP keys and required different versions of the driver.

Using Windows to search for driver updates for the HASP USB keys used for InteractX licensing can result in Windows installing SafeNet Inc Sentinel drivers. Note when InteractX is installed, it already includes drivers for the HASP USB keys, named Aladdin. 

This can sometimes happen due to Windows updates or more likely if you plug the HASP USB key in after Windows is booted.  With default Windows 7 settings Windows may go out and automatically try to search/update the HASP driver and find and install the incorrect one (Sentinel/Safenet).  Here is a way to change the settings in Windows 7 to prevent Windows from automatically searching/updating device drivers:

How to stop Windows 7 automatically installing drivers

However, if you've already installed the Sentinel, they're not easily uninstalled. Simply deleting them from Device Manager does not remove them from Windows. Here's a video on youtube.com that shows SafeNet's video on how to remove the Sentinel drivers.  Note SafeNet Inc is a separate company and in no way is affiliated with Parker Hannifin Corp. This information is given as convenience for users to fix their computers.  Parker is not liable for user's computers. You may contact SafeNet for latest product updates and support procedures.

SafeNet video on youtube.com:  How to remove Sentinel HASP Runtime Installation

Also note,  in limited testing, the SSDCleanup utility from SafeNet in testing was not reliable in removing the drivers from a Win7 64bit pc but the procedure in the above video was successful.

 

If installing InteractX and the Sentinel drivers have already been installed, you'll see an error that looks like this:

The Aladdin drivers are not a separate installation and are part of InteractX software. So you'd need to cancel the installation and re-run it.  Installing InteractX requires restarting your PC and is not complete until after rebooting your PC and then InteractX will then finish the install.

When installed Windows will then notify users:

Within Device Manager, the Aladdin drivers will appear under the USB controllers:

 

HASP SRM Run-time Environment

8/4/15jh

glh 10/2015

dm08032018

  • Windows 10
  • Windows 7
  • InteractX
  • Sentinel
  • Compatibility
  • Installation
  • Hasp
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply