Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base PAC CNC & Multi-Axis Capabilities, Samples & Video demos
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base PAC CNC & Multi-Axis Capabilities, Samples & Video demos
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
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
  • AC/DC Industrial Drives+
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
PAC CNC & Multi-Axis Capabilities, Samples & Video demos

Print Friendly and PDF

The PAC controller has Motion, Logic, CNC and Visualization integrated into one platform. It can be programmed in Ladder Logic (LD), Structured Text (ST), Sequential Function Chart (SFC), Continuous Function Chart (CFC). From these programs, multi-axis coordination can be commanded, using PLCopen SoftMotion function blocks. The CNC section supports industry standard DIN 66025 CNC G-code. This allows users to select different parts through different G code files.

The PAC has pre-defined for kinematic transformations for common mechanic systems. This allows users faster machine startup. Users only need to define the different lengths of their actuators and these function blocks are used within the PLC code similar to other motion or logic function blocks within the same environment.

  • This video demonstrates a delta bot and that logic: MOBILE USERS CLICK HERE

The PAC also offers a Web Visualization for CNC applications. This allows 2D or 3D visualizations on the PAC Terminal or a web browser.

  • This video demonstrates Web Visualization for CNC: MOBILE USERS CLICK HERE

Below are multiple sample projects. Select the projects that match your version of Parker Automation Manager. These can be ran with or without a physical PAC device (simulation mode in PAM1.4, or a virtual Codesys device in Pam1.2/PAM1.3).

Video of one of the projects: MOBILE USERS CLICK HERE

PAM1.4:

  • CNC_File_3DPath__Gcode_Vis_PAM1.4
  • CNC_File_PAM1.4
  • Displaying G-code while running, as well as the path: CNC_Sample_PAM1.4
  • 2-axis Gantry Interpolation from CNC Gcode with Visualization: CNC_direct_PAM1.4  - Video demonstration: MOBILE USERS CLICK HERE

PAM1.2

  • CNC_File_3DPath_GcodeVis_PAM1.2
  • CNC_File_PAM1.2
  • Displaying G-code while running, as well as the path: CNC_sample_PAM1.2
  • 2-axis Gantry Interpolation from CNC Gcode with Visualization: CNC_direct_PAM1.2  - Video demonstration: MOBILE USERS CLICK HERE

Below are screenshots that provide at-a-glance CNC capabilities:

Standard G code can be viewed and edited within the software:

Programmers can import into the CNC in the PAC software from .dxf or from ASCII file:

5-Axes Transformation

2-Axes and 3-Axes Gantry

2-Axes and 3-Axes with Cutter

H-Gantry with Stationary Drives

T-Gantry

Polar:

2-jointed or 3-jointed SCARA:

Tripod / Bipod:

4-Axes Palletizer:

6 Degree of Freedom (6DoF) Articulated Robot:

Users can also define their own mechanical systems and the PAC has the processing power to do kinematic transformation on the fly, such as for a Stewart platform (6 Degrees of Freedom). For additional information, contact factory at emn.service@support.parker.com

10/12/15jh

1NOV18 JD

20SEP2021 DCLIFFE - Updated links to HTTPS and updated metadata.

  • PAC
  • code
  • CNC
  • MULTI
  • g
  • AXIS
  • sample
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply