Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I determine the MAC address for my unit?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I determine the MAC address for my unit?
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
  • General Technology Information-
    • How do I determine the MAC address for my unit?
    • Install the network card in Windows NT.
    • Servers Services error on boot up in NT
    • Comparison of Motor Technologies: Servo, Stepper, Stepper with Encoder
    • How to check if a USB to serial converter has an FTDI chipset
    • Modbus Basics
    • Recommended Installation Practices for Robust Systems
    • Video: Different Servo Loop Control Schemes, Drives with Fieldbus vs Motionbus
    • Video: Electric Motors Overview: Brushed, Stepper and Brushless
    • Video: Gearhead Engineering Reference
    • Video: How a Brushed Motor works
    • Video: How a Drive controls current in a stepper or servo motor
    • Video: How a Servo Motor works
    • Video: How a Step Motor works
    • Video: How is a Brushed Motor Constructed?
    • Video: How is a Servo Motor Constructed?
    • Video: How is a Step Motor Constructed?
    • Video: How Servo Loops and PID works (Torque, Velocity, Position)
    • VIDEO: How to set your PC's Ethernet IP address
    • VIDEO: How to troubleshoot RS232 serial communications
    • Video: IO Wiring: What is NPN PNP Sinking Sourcing?
    • Video: Servo Motor Feedback (Encoders, Halls & Resolvers) & Commutation
    • Video: Step Motor Resonance
    • Video: Step Motor Windings explained: Series vs Parallel
    • What is EtherCAT? How does it work? How does it help me?
    • What is IEC61131-3? What is PLCopen?
    • Windows 10 support (Win10)
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
How do I determine the MAC address for my unit?

Print Friendly and PDF

There are two ways to determine this.  The direct method and the indirect method.

The direct method requires that you know the IP address of the unit and have a physical Ethernet connection to the unit.  From a PC (Windows) open a command dialog (cmd entered in the Start button 'Search program and files' box).  From the command dialog  you may be familiar with the "ping" function.  Another useful utility is the "arp" function.  In this case you can use it to get the MAC address back from the unit.

In the command dialog enter the following:  arp -a 192.168.10.43

(192.168.10.43 indicates the IP address of the unit so replace with the IP address of your unit).

The response will be in hexadecimal and listed as Physical Address.  See screen shot for ping and arp examples.

 

The indirect method is to contact us at emn.service@support.parker.com (or call 800-358-9068) with the serial number from the unit.  Our Applications Engineering (technical support) group can look up that serial number to see what MAC address was assigned.

 

 

glh 11/2015

  • IP Address
  • Ping
  • Network
  • MAC ID
  • ARP
  • Ethernet
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply