Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base FTP support
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base FTP support
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
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
FTP support

Print Friendly and PDF

Is it possible to access the USB port by FTP?

Yes, the entire file system is accessible over FTP including the RAM drive, SD card and USB thumbdrive(s) if any are plugged in. Currently, the FTP server is available on all PAC models running firmware 1.3.0 or higher. Xpress user administration controls the user permissions. The default account is Admin with a blank password.

You can access the FTP server using Windows File Explorer or Internet Explorer. Internet Explorer will allow you to download files, but File Explorer will also allow you to upload files, delete files and add/delete folders. You can access it using network file addresses like the ones given below.

IMAGE BROKEN -- DCLIFFE

Examples:

ftp://Admin@172.25.8.25

ftp://Admin:Password@172.25.8.25

ftp://Admin@192.168.10.50 (default for X2 port)

SD Card Path

ftp://Admin@192.168.10.50/System/Hard Disk

External USB Drive Path (first drive found)

ftp://Admin@192.168.10.50/System/Hard Disk2

External USB Drive Path (second drive found)

ftp://Admin@192.168.10.50/System/Hard Disk3

PAC RAM Drive

ftp://Admin@192.168.10.50/System/

Note the project and firmware resides on the SD card and thus users need to be careful writing to the SD card. The preferred method of storing files on the PAC is to transfer them down to a USB stick that resides in one of the PAC's USB ports. The drive should be formatted as FAT32.

Sometimes, users may want to transfer down a file that is intended to be temporary. Examples include CNC files, recipe files and other files that may be useful in the process. In this case, it is often better to transfer the file to the RAM drive instead of a USB stick. This is because the RAM drive is faster than USB and will not wear out over time like the flash cells in a USB drive will. Note that all files stored in the RAM drive are lost when the PAC powers down.

Is it possible to define a default directory for FTP access, which is active after a FTP connection has been established?
No, currently it is not possible but is something that we could add in the future.

The FTP server is also available on PACs running firmware 1.2.1 or 1.2.0 that have an X or B in their model number as shown below:

PAC320-PXN21-3A
PAC320-PXE21-3A
PAC320-PXP21-3A
PAC320-PXB21-3A
PAC320-MXN21-3A
PAC320-MXE21-3A
PAC320-MXP21-3A
PAC320-MXB21-3A
PAC320-CXN21-3A
PAC320-CXE21-3A
PAC320-CXP21-3A
PAC320-CXB21-3A
PAC320-PBN21-3A
PAC320-PBE21-3A
PAC320-PBP21-3A
PAC320-PBB21-3A
PAC320-MBN21-3A
PAC320-MBE21-3A
PAC320-MBP21-3A
PAC320-MBB21-3A
PAC320-CBN21-3A
PAC320-CBE21-3A
PAC320-CBP21-3A
PAC320-CBB21-3A

11/19/15jh

UPDATED 19MAY2017 DC

-->