Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)

Print Friendly and PDF

Beginning with firmware version 4.42 IPA servo drive controllers support BiSS-C and BiSS-B encoder feedback.

Parameter C171 tells the drive what feedback will be connected.
C171=5 for BiSS
when C171 is changed, the drive needs to be power cycled or issued the REBOOT command to implement the change.
ACR-View 6.4.1 supports BiSS feedback. Prior to downloading the motor file ACR-View will check the current value of C171 and if the new value is different a REBOOT command will be issued following the motor file download to enable the new settings.
in addition to C171 three other parameters are required for BiSS set-up.
Parameter Description
C168 Number of valid bits= single turn + multi turn
C179 Set-up value
C180 Multi-turn value


These parameters are included as part of the motor file download in ACR-View for the following Parker motors.

Parameter C168 C179 C180
Description valid bits Set-up value Multi-turn value
PM-FAL w/o battery 34 37752853 65535
PM-FBL w/o battery 35 37752853 65535
PM-FCL w/o battery 35 37752853 65535
PM-DD 20 41943061 1
MX80L 26 33554458 1
PM-FAL w/ battery 34 33558549 65535
PM-FBL w/ battery 35 33558549 65535
PM-FCL w/ battery 35 33558549 65535

BiSS ENCODER PIN-OUT
IPA Pin BiSS Function P Encoder cable Wire
1 SLO WHITE
2 /SLO WHITE w/black
3 Encoder power return ORANGE w/black
4 +5 VDC Encoder power ORANGE
9 MA yellow
13 /MA yellow w/black

Pre-made cables are available for IPA and P Series motors:
Cables to connect P series rotary motors to IPA series drives:
  • 71-032647-xx.....Encoder cable, Single-turn, xx length in meters 03, 05, 10, 20
  • 71-032751-xx.....Encoder cable, Multi-turn, xx length in meters 03, 05, 10, 20
  • 71-032681-xx.....Encoder cable, Single-turn, HIGH FLEX, xx length in meters 03, 05, 10, 20
  • 71-032752-xx.....Encoder cable, Multi-turn, HIGH FLEX, xx length in meters 03, 05, 10, 20
Cables to connect P series Direct Drive PM-DD rotary motors to IPA series drives:
71-032648-XX.....DD Motor feedback cable, xx in meters 03, 05, 10, 20
Feedback power is maintained by the IPA. If the battery fails, the IPA with fault with a feedback fault and the motor cannot be enabled until the battery is replaced.
The battery is only used while the IPA is powered down and thus under normal use will last 5years+ before needing replaced.


jw-sept 2016