Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX Upgrades
      • InteractX Misc - How to re-register older versions of Interact X (versions 1.x through 3.4)
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline

Print Friendly and PDF

CIP for ACR9000 / Aries CE

In cases where there are more than one CIP device, (HMI, PLC, etc...) they share a single data stream in the controller. We keep track of how many devices connect to the data stream and when they all disconnect we close the data stream.

There is currently an issue in ACR / Aries CE OS versions up through 2.41 which can cause the data stream to be closed and CIP communications stops even though there are devices still using it. The count of devices is incorrectly decremented by two when a device goes offline which results in a zero count when devices are still attached. If you are using just one CIP device, this issue will never be a problem. If you have multiple devices and just one of them goes offline several times, all devices will loose their connection.

To recover communications, ether the controller must be power cycled so that it re-initializes the CIP device count, or all of the CIP devices must be shut down then all restarted which will allow the controller to detect the correct number of devices.

The issue has been identified and will be fixed in a future release.