The zip file in the link below will show the reader how to develop a CNC machine with the PAC that reads G code from a file stored on a drive on the PAC. It contains an application note, a PAM project archive, a DIN66025 compliant G code and an embedded Xpress LRP file that can be used to run the sample.
To see more CNC capabilities please see other FAQ pages on the same subject, available under the "PAC" heading on the left side of the page.
Select the project that matches your version of Parker Automation Manager:
PAM1.4: CNC_From_File_Example_PAM1.4
PAM1.3: CNC_From_File_Example_PAM1.3
DC 14MAR2016
Updated DC 16MAR2016
WebVis example 22JUL2016
Updated Project Archive for v1.30 GLH 3/13/18
1NOV18 JD -1.4 update - Mentioned other FAQ pages - Title Clarity