The maximum drive operating altitude is 5000m (1640 ft.). Note: The drive has to be derated linearly 1% per 200 meters above 500m to a MAXIMUM of 5000m (16400 ft.).
- For more information on derating the drive at higher altitudes see this quick link to the 590+ on Parker.com - Manual, QuickStarts, Product Support, etc
14JUN2016 LS