Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • 590+ - Transferring a Configuration to a Drive with a Different Power Level
      • 598/599+ Stack Controller Replacements
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • HOW DO I CONVERT DC590+ UK/JDE PART NUMBERS TO US PART NUMBERS?
      • Speed Regulation with 590+ Drives
      • Troubleshooting a DC brushed motor
      • What are differences between a Regen and Non-Regen 590+?
      • What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
      • Why is every light on the keypad flashing on my 590+?
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x?

Print Friendly and PDF

This document will explain how to upgrade a 590+ Frame 1 or Frame 2 with firmware v5.x or v7.x to a v8.x. control board, and migrating the configuration. This is not a firmware update for an existing control board. This is an entire replacement of the control board to upgrade to a newer major revision, on the Frame 1 and 2 that utilizes the control "cradle" design.

  • To update to newer minor revisions of firmware use the DSELite software.
  • To update to newer major revisions of firmware, you must replace the control board.

  • Link to document
[QuickLink for the 590+ on Parker.com] - Manual, QuickStarts, Product Support, etc
21JUN2016 LS
30May19 JD
  • board
  • Install
  • Upgrade
  • firmware
  • 590+
  • control