Go to Parker.com
Search
Sign in
Technologies
Aerospace
Climate Control
Electromechanical Group
Filtration
Fluid and Gas Handling
Hydraulics
IoT
Pneumatics
Process Control
Sealing and Shielding
Other Groups
Parker Indego
Blogs
Forums
Knowledge Bases
Parker Community
Technologies
Aerospace
Climate Control
Electromechanical Group
Filtration
Fluid and Gas Handling
Hydraulics
IoT
Pneumatics
Process Control
Sealing and Shielding
Other Groups
Parker Indego
Blogs
Forums
Knowledge Bases
Search
User
Site
Search
User
Home
Technologies
Electromechanical Group
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base
Why is my DC motor running hot?
Technologies
Electromechanical Group
Electromechanical - Industrial
More
Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base
Why is my DC motor running hot?
Electromechanical – Industrial Support Forum
Electromechanical Industrial Knowledge Base
Members
Sub Groups
More
Cancel
New
Electromechanical - Industrial requires membership for participation - click to join
Electromechanical Knowledge Base & Frequently Asked Questions
+
Motion and Machine Controllers
+
General Technology Information
+
Virtual Engineer
+
Visualization and Human Machine Interface (HMI)
+
Servo Drives and Servo Drive/Controllers
+
Stepper Drives and Stepper Drive/Controller
+
Gearheads
-
AC and DC Drives and Inverters
+
AC10
+
AC30
+
AC690+ Series
+
AC890 Series
-
DC590+ Series
How do I start troubleshooting a 590+?
What are the basic wiring connections required to run a motor, using the factory default drive?
How to Extract and Install Parameters to the 590+ Drive using DSE Lite
Why won't my motor run?
How can I make sure my DC motor does not have a problem with the Field Windings?
Why is my DC motor running hot?
590+: Is the keypad detachable during operation?
Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
Can you download a DSELite file into the drive when the drive is running?
How can I get the DSELite software the 590+ uses?
How can I make sure the motor will not start rotating until the speed pot is at 0?
How can I manually tune a 590+ drive to my motor?
How can I pre-trip "speed feedback" alarm before the drive trips?
How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
How can I set up a 590+ to be a field controller?
How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
How can the 590+ be programmed?
How can the drive configuration be reset to factory defaults?
How do I clone my 590+ Drive with the keypad?
How do I copy the configuration of one drive to another using the keypad?
How do I flash my 590+ drive to a newer Minor Revision of Firmware?
How do I know what firmware revision my 590+ is?
How do I set up a 590+ External Stack?
How to I configure the 590+ for Preset Speeds?
Is there anything I can check for a SEQ PRE READY alarm?
Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
The 590+ is enabled, but the main contactor doesn't close. Why?
Upgrading a control door from a 590 to a 590+
What accessories can be added to the 590+?
What analog and digital I/O is available on the 590+?
What are the Communication options for the 590+?
What are the communication settings for the 590+ for the P3 Port?
What are the differences between the 590 and 590+?
What are the minimum and maximum 3phase input ratings for the 590+?
What are the reference power supplies available to terminal connections on the 590+?
What are the types of Speed Feedback for the 590+?
What is the current overload rating for the 590+ drive?
What is the maximum operating altitude for the 590+?
What is the operating temperature for the 590+?
What safety standards does the 590+ meet?
What USB-serial adapter should I use?
Why does the drive fault to "Over-Voltage" after the drive is enabled?
Why does the drive fault to "speed feedback"?
Why does the drive fault to 3 phase-fail after the drive is enabled?
What I can I check for a CALIBRATION FAIL trip?
590+ - Transferring a Configuration to a Drive with a Different Power Level
598/599+ Stack Controller Replacements
DC590+ Encoder Feedback Card Options
DRV Contactor Options (955+ part numbers)
How do I convert DC590+ Europe part numbers to US part numbers?
Speed Regulation with 590+ Drives
Troubleshooting a DC brushed motor
What are differences between a Regen and Non-Regen 590+?
What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
Why is every light on the keypad flashing on my 590+?
+
TS8000, DSI3, & DSI8000
+
Legacy/Discontinued VFD Products
What software and communication cable are used for programming?
DSE Lite and Drive Firmware Compatibility
How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
Why does DSE or DSELite crash when creating or opening a new project?
How can I flash the LinkNet Techbox firmware?
What is an Autotune and how do I run one?
Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
6053...6054...6055...? Techbox options
How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
Maximum Speeds for VFD drives
Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
What is 'BOOST' in Parker VFD drives?
+
Servo Motors
+
Step Motors
+
Linear and Rotary Positioners
+
Electric Cylinders
+
T-Slot Aluminum Framing
+
C3 + Xpress + ETH
How can I stay updated on Parker electromechanical and drives product news?
+
Legacy (Discontinued)
+
Other
Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
What replaces the Gemini GV6K servo drive controller?
Why is my DC motor running hot?
Revision
Creation Date
Revision Author
Select All
Current Revision
9 Dec 2019 6:19 PM
Jack DeGrano
7
Revision #7
13 Jun 2019 11:01 PM
Jack DeGrano
6
Revision #6
13 Jun 2019 11:01 PM
Jack DeGrano
5
Revision #5
13 Jun 2019 10:57 PM
Jack DeGrano
4
Revision #4
13 Jun 2019 10:57 PM
Jack DeGrano
3
Revision #3
5 Jan 2018 12:08 AM
William Chin
2
Revision #2
12 Dec 2017 3:42 AM
William Chin
1
Revision #1
1 Oct 2017 9:50 AM
Electromechanical and Drives Team
Compare Versions
View current version