Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Using analog PACIO modules
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Using analog PACIO modules
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware-
        • How do I order a replacement SD card for my PAC controller?
        • No Boot Device Found
        • PAC320 and PACIO Replacement Hardware
        • PACIO Connector Part Numbers
        • Using analog PACIO modules
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
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
Using analog PACIO modules

Print Friendly and PDF

There are several PACIO modules available that are designed for analog signal processing. These are:

Model Number Type Description
PACIO-441-01 AI4-mA 12 Bit Four single-ended 0..20mA or 4..20mA analog inputs.
PACIO-441-02 AI4/8-VDC 13 Bit Eight single-ended or four differential 0..10V or +/-10V analog inputs.
PACIO-442-02 AO4-VDC/mA 12 Bit Four 0..10V, +/-10V, or 0..20mA analog outputs.
PACIO-443-01 AI4-Pt/Ni100 16 Bit Four Pt/Ni100 temperature sensor or resistance measurement inputs.
PACIO-443-03 AI4-Pt/Ni1000 16 Bit Four Pt/Ni1000 temperature sensor or resistance measurement inputs.

These function blocks all read or produce analog signals as integer values, which means that the values must be scaled and converted to or from REAL or LREAL floating point formats in order to be truly useful. To make this easier, this FAQ includes a link to download a set of function blocks that show how this is done. Many users will be able to drop them into their programs without modification.

The function block library can be downloaded below, the library comes with a basic example for each module showing how it should be used. Select the library that matches your version of Parker Automation Manager:

PAM1.4: Analog_PACIO_Library_PAM1.4

PAM1.2: Analog_PACIO_Library_PAM1.2

Tips:

  • Some modules have Unipolar and Differential settings. If you are operating the module in Unipolar mode, set the bUnipolar input to TRUE on the helper block.
  • Test the full range of the analog input and make sure your program can properly read accurately read values from the entire range. If not, make sure you are operating the input or output in the right mode.
  • If you install the provided library, you can view the source code (great for debugging) by double-clicking the block after you put it into CFC or Ladder. In Structured Text, you can right-click it and click "Go to declaration".
  • If your measured voltage, current, or temperature value appear to be bouncing around, consider activating the filter built into each channel. This can help to stabilize the value. Some applications may also require additional grounding and noise-mitigation measures. PACIO modules can be equipped with a shield bond to enhance noise-immunity of shielded I/O cables. Model numbers for the shield bonds available are PACIO-412-01 (single position) and PACIO-412-02 (dual position). See page 138 of the PAC User Guide for more information.
  • Analog input and output modules all have multiple options for how they may be used. All of these options are implemented as simple state machines that can be triggered with the SetOptions bit in their PDO (Process Data Object) maps. By default, the units power up with all inputs and outputs disabled to prevent shorts. An example of how to enable them and set options can be found in the library download link given above.

07OCT2016 DCLIFFE

30OCT18 JD

15FEB2021 DCLIFFE -- Updated links to HTTPS.

  • analog
  • PACIO
  • PAM
  • module
  • library
  • sample