Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
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
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?

Print Friendly and PDF

The 1002-00 can be used as both a cloning module and serial converter to use with DSELite. To use as a cloning module see this FAQ: Cloning with the 1002-00

For the free DSELite software download see this FAQ.

If you need to manually download drivers for the device, they can be downloaded here: Module Drivers v2.12.06.zip

This FAQ assumes you have all of the small components that come with the 1002-00 part number for some potential reasons mentioned below. Parts that come with the 1002-00 part number and information on the module are below:

 

Important Notes:

  • Verify the firmware version of the drive. Parameter F105 is the firmware version. It is important to know if you can use DSELite, and to know the template version to use later on. It is not possible to flash firmware on an AC10 in the field. 
  • Firmware compatible with DSELite: 
    • IP20 Frames 1-5 with firmware 2.00, 2.27, 2.31 or later
    • IP20 Frames 6-12 with firmware 3.27 and 3.31 or later
    • IP66 All Frames: 4.27 and 4.31 or later

  • The module requires +5V: The serial converter will be plugged into a PC during operation, your PC is capable of supplying this +5V signal with, or without, the AC10 powered via it's own AC mains.
  • If your AC10 has a green serial terminal you may connect the module directly into the drive (and the cable can be used to extend it, as shown below, if horizontal space next to the drive is limited). Old models of the IP20 drives, that were less than 22Kw, may not have a green serial port. If this is the case, you will be to use the AC10 module as the other port is only used for external keypad use. You must manually take note of all parameters being used to reprogram your new drive.

  

  • Several parameters in the drive must temporarily be set to default values (and then changed back to application-dependent values after loading them into the new drive). 

AC10 Port Locations:

  1. [IP20 < 22Kw] 
  2. [IP20 > 22Kw] 
  3. [All IP66]

Connecting the tool as a serial converter with DSELite:

Wiring the tool to the PC and AC10:

  • AC mains is not required

Setup Computer COM Port in DSELite:

  1. Verify the COM port being used on the PC via device manager
  2. Launch DSE Lite
    • Make sure the device is plugged in before doing so. DSELite scans its communication ports at startup.
  3. Go to the COM port Icon
  4. Make certain the AC10 Support is selected
  5. Make certain the Baud is set to AUTO
  6. Make certain the correct COM port is selected
    1. Once selected, you should see the scratchpad display the last line (click for clarity):

Using DSELite:

  1. Open an AC10 template that matches your drive frame, and firmware version (see the above picture).
    • The pre-baked template variant does not matter here. When you extract into any template with step 2, it will overwrite the template you have open.
  2. Command -> Extract Drive Parameters will extract your configuration and parameters into the template, and overwrite it
    • You must have an AC10 template open that matches your drive frame, and firmware version
  3. Command -> Install will install your configuration and parameters into the drive (you will need to implement motor data and run an autotune if in SLV mode).
    • Command -> Full install is only used when you are installing into an identical AC10 that the configuration was originally extracted from; as it installs frame dependent information.

  • When using DSELite and a parameter is changed while in the On Line Mode (Command -> Online), the parameter will automatically be saved. 
  • If you want a list of the Modbus Registers do a File / Document and at the end of the document there will be Parameters by Register (Modbus)

[QuickLink for the AC10 on Parker.com] - Manual, QuickStarts, Product Support, etc

15OCT19 JD

  • DSELite
  • 1002-00
  • Serial
  • AC10
  • Extract
  • converter
  • Download
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply