Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX
      • InteractX Misc - Re-register older versions of Interact X (versions 1.x through 3.4) NO LONGER SUPPORTED
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
      • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
      • InteractX Misc - How to Edit Text Alt+Double-click
      • Reading and Writing Allen Bradley Logix tags that are strings
      • Serial Communications Driver error on Com1 on boot of the runtime system.
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.

Print Friendly and PDF

The symptom on the run time system will be a loss of the characters on some of the keys or buttons on the pop-up keyboard, pop-up keypad, selection list tool, logon tool, verification tool, authentication tool, user admin tools, etc. 

The application looks fine under the development system but then after transfer to the run time most of the button labels are blank (though a few things will still show up like the numbers on the keypad).  See pictures below for some examples.

This symptom is created by attempting to download the Interact X run time along with the Application Files on Windows 7 systems.  This feature is a carry-over from older versions of InteractX and was intended as a method of upgrading the run time when needed to match your development version as long as your run time license was still valid.

However, this no longer functions correctly on Windows 7 systems due to the tighter system security that Windows 7 uses and one of the symptoms that results in it losing track of the character map for all of these pop-up type tools.  Parker strongly recommends that you do not download the runtime from the development software, only the Application Files are needed to get your application to the run time system. 

The runtime version does need to match the version that the project is developed in.  So, if you do need to update the run time version, you should manually un-install it and then install the newer version not use the transfer option from the development software to do this.  It will cause corruption of the run time software and require un-installing and re-installing the run time or re-imaging the entire drive.

Fix - as stated above, once the run time has been corrupted there is no easy solution.  You will need to either un-install and then re-install the run time software or re-image the entire drive.  If you re-image the entire drive using the Acronis recovery software (either on the Parker IPX or Parker IXA models) it will restore the factory default image including the original run time.  Any other software that had been installed will then need to be re-installed (like the Interact X application itself). 

keyboard example

keypad example

 

logon example

selection list example

missing characters on Interact X pop-up keyboard missing characters popup keyboard missing characters pop-up keypad missing characters popup keypad missing characters logon missing characters selection list missing characters log viewer missing characters alarm tool missing characters input list missing characters

glh 3/2017

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply