Go to Parker.com
  • Sign in
Technologies
  • Aerospace
  • Climate Control
  • Electromechanical Group
  • Filtration
  • Fluid and Gas Handling
  • Hydraulics
  • IoT
  • Pneumatics
  • Process Control
  • Sealing and Shielding
Other Groups
  • Parker Indego
Blogs Forums Knowledge Bases
Parker Community
Parker Community
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
    Other Groups
    • Parker Indego
    Blogs Forums Knowledge Bases
  • User
  • Site
  • Search
  • User
Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base AC10: Why is my AC motor running hot?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base AC10: Why is my AC motor running hot?
  • Electromechanical – Industrial Support Forum
  • Electromechanical Industrial Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical - Industrial requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • DC590+ Series+
    • AC890 Series+
    • AC15/AC20
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners+
  • Electric Cylinders+
  • T-Slot Aluminum Framing+
  • C3 + Xpress + ETH+
  • How can I stay updated on Parker electromechanical and drives product news?
  • Legacy (Discontinued)+
  • Other+
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
Wiki Actions
  • Share
  • More
  • Cancel
Community Quick Links
  • Home
  • Technologies
    • Aerospace
      • Supplier Resource Center
    • Climate Control
    • Electromechanical Group
      • Electromechanical - Industrial
      • Electromechanical – Mobile
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
      • Pneumatic Industrial
      • Pneumatics Mobile
    • Process Control
    • Sealing and Shielding
  • Other Groups
    • Parker Indego
      • Parker Indego Instructors
      • Parker Indego Therapists
      • Parker Indego Distributors
  • Community Blogs
  • Community Forums
  • Community Knowledge Bases
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

AC10: Why is my AC motor running hot?

Print Friendly and PDF

  1. MOTOR CONNECTIONS:
    1. Make sure the motor is rated for inverter-duty.
      1. Motor drives are not transformers. The voltage you apply to the input mains is often the max PWM voltage on the motor. The PWM signal is modulated such that you get a nominal rating to provide motor control.This is a principle of PWM control. If your AC mains is 460Vac, and your motor is rated for 230Vac, and not inverter-duty rated  there is a strong chance the motor will not live its full life.
    2. Make sure the stator is properly connected for the voltage provided by the inverter.
    3. Make sure there are no loose motor connections.
  2. INVERTER SETTINGS:
    1. For SV Mode, make certain the magnetizing current is not set too high.
    2. For V/Hz mode, make sure the boost is not set too high.
  3. RUNNING CONDITIONS:
    1. Is there a Blower on this motor?
      1. Are the blower filters clogged?
      2. Is there free airflow through the motor?
      3. What is the ambient temperature?
    2. Does the motor run below 25% speed for extended periods of time (without forced air cooling)?
    3. Is the motor running with the motor torque >75% for extended periods of time (without forced air cooling)?

[QuickLink for the AC10 on Parker.com] - Manual, QuickStarts, Product Support, etc

28NOV2016 LS

11SEP19 JD

  • motor
  • hot
  • running
  • AC10
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Related
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Parker Hannifin Parker Hannifin

  • Products
  • About Parker
  • Investors
  • Community
  • Careers

Global Operations Global Operations

  • Divisions
  • Sales Companies
  • Worldwide Locations
  • Distribution Network
  • ParkerStore™ Network

Company Information Company Information

  • Newsroom
  • Event Calendar
  • Working with Parker
  • Product Brands
  • History

Global Support Center Global Support Center

  • Support
  • CAD
  • Where to Buy
  • Contact Parker
  • Manage Online Orders
© Parker Hannifin Corp 2023
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.