Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How to receive ASCII data
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How to receive ASCII data
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
How to receive ASCII data

Print Friendly and PDF

The example below is an alternative the INPUT command in the ACR controller. The routine will read one ASCII character at a time from the PC or other device. To end the transmission from the third-party controller, we look for a carriage return  (ASC 13) as in  IF (ASC($V0)=13) within the ReceiveData subroutine. This can then allow the programmer to continue program execution if desired as compared to the INPUT command which inhibits program execution.

Notes: The ACR9000's USB port uses Stream1. If using Ethernet, ACR-View will connect to the first available of the 4 streams (Stream2 - 5).

To see the stream number when connected, type STREAM

Below sample uses Stream#3 while leaving ACR-View with Stream#2 connected. This will not run from ACR-View's terminal emulator. Use connect via HyperTerminal or Putty (use Port 5002 which is the ASCII port)

If testing with PBOOT within the program, use ACR-View and CLOSE #3 before doing a REBOOT command to test the power-up function.

PROGRAM
DIM LV4
DIM $V(10,50)
OPEN "STREAM3:" AS #3 : REM Open communication to PC
_loop
print #3, "enter something"
$V2="" : GOSUB ReceiveData
print #3, "something is: ",$V1
goto loop
 

_ReceiveData
$V1=""
WHILE (3)
 IF (KBHIT(3))
 $V2=GETCH(3)
 IF (ASC($V2)=13)  : rem ASC 13 is carriage return
  BREAK  : REM Break out of the WHILE loop
 ELSE
 $V1=$V1+$V2
 endif
 endif
WEND
RETURN
ENDP
 
jw 12/2016
updated 3/7/17jh
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply