Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I set up an AC10 for torque control?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I set up an AC10 for torque control?
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
  • AC and DC Drives and Inverters-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • AC10 Modbus-RTU Example to Interact Xpress HMI (XTA)
      • Can an AC10 run a PMAC motor?
      • How does the password protection feature work in the AC10 (via DSE Lite)?
      • How does the password protection feature work in the AC10 (via the keypad)?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • When I try to Install or Full Install from DSE Lite to my AC10 nothing happens.
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
How do I set up an AC10 for torque control?

Print Friendly and PDF

Although torque control on the AC10 is certainly possible in Sensorless Vector mode, its primary functionality is to be used in velocity-type applications with torque compensation rather than direct control.

For Sensorless Vector torque control (of AC induction motors) we advise using the 690+, 890 drives, or AC30 drives. More information can be found on this FAQ site under their respective sections in the sidebar, or on their respective product pages on Parker.com.

If you think you have a volume application that requires an AC10 in torque control please contact your local Parker ATC, or Parker Applications for advisement.

Equipment needed: AC10 drive, AC10 Manual

[QuickLink for the AC10 on Parker.com] - Manual, QuickStarts, Product Support, etc

Procedure:

  • Control Mode MUST be set for Sensorless Vector for Torque Control
  1. Set AC10 parameters as follows.

    Parameter Description Setting Range Default
    F106 Control Mode 0: Sensorless Vector
    1: Reserved
    2: VVVF (V/Hz)
    Vector Control 1
    2
    F228 Application Selection 0: Invalid
    1: Basic Speed Control
    2: Auto/Manual Control
    3: Stage Speed Control
    4: Terminal Control
    5: PID Control
    0
    FC00 Speed/Torque Control 0: Speed Control
    1: Torque Control
    2: Terminal Switchover
    0
    FC06 Torque Given Channel
    (Torque Command Source)
    0: Digital Given (FC09)
    1: Analog Input 1
    2: Analog Input 2
    0
    FC07 Torque Given Coefficient
    (Torque Command Scaling)
    0.1
    (Start here and adjust upward as required)
    3.000
    FC06 Torque Offset Channel
    (Torque Offset Source)
    0: Digital Given (FC17)
    1: Analog Input 1
    2: Analog Input 2
    0
    FC07 Torque Offset Coefficient
    (Torque Offset Scaling)
    0.5 0.500
    FC17 Torque Offset 0 10.00
  2. Ensure required motor information and I/O setup for your application is followed. (Is there an enable, an external fault, etc etc).
  3. Perform a rotating autotune on the connected motor for Sensorless Vector mode.

3JAN2017 LS

12SEP19 JD - Update

  • AC10
  • torque