Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Misc - Uploading and downloading InteractX projects with a USB drive
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Misc - Uploading and downloading InteractX projects with a USB drive
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX Upgrades
      • InteractX Misc - How to re-register older versions of Interact X (versions 1.x through 3.4)
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
InteractX Misc - Uploading and downloading InteractX projects with a USB drive

Print Friendly and PDF

There are three ways to transfer an InteractX application to or from an industrial PC running an InteractX runtime: disk (USB drive), Ethernet and serial. This FAQ will cover USB since that is the one that is typically recommended for novice users of InteractX. This procedure applies to the following Parker (CTC) HMI model lines:

  • PX
  • HPX
  • EPX
  • EPX2
  • IPX
  • IXA

For this method, you will need a laptop/desktop with MachineShop Suite installed on it. While uploading and downloading applications does not require a license, you will need one if you intend to do any editing of the application.

[Related FAQ: Uploading and downloading InteractX projects over Ethernet]

Transferring an Application from the HMI to the Development PC

This method will allow you to deploy or retrieve an application in the event that your HMI is not connected to a network or you are having network connectivity issues. You will need a USB stick for this method, preferably one with 1 GB or more of free space.

Step 1: Exit Runtime

On your HMI, exit the InteractX runtime. There are several ways to exit the runtime, but it is possible for an application developer to turn off any or all of them. You may need to try more than one of these options:

  • Press an Exit button in the application.
  • On a keyboard, press Alt+F4.
  • On a keyboard, press Ctrl+Alt+Delete. From there, open Task Manager and kill the HMIRun.exe process.

If none of the above options work, call 707-584-7558 or email emn.service@support.parker.com

Step 2: Locate the Deployment Server

Now that you are on the desktop of your InteractX HMI, look in the task bar near the bottom right-hand corner of the screen. You should see a small icon in the taskbar that looks like a bowling ball. This is the icon for the Deployment Server.

IMAGE BROKEN -- DCLIFFE

Step 3: Right-Click the Deployment Server

Plug in your USB drive and wait a few seconds for the HMI to recognize it. Right-click the Deployment Server icon and click Upload Applications to Disk in the option box that appears.

IMAGE BROKEN -- DCLIFFE

Step 4: Select a Drive

In the dialog box that appears, click Browse. Select the directory on the USB drive to which you would like to upload the InteractX application.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Click OK and then click Finish. The Deployment Server will upload your application to the disk and notify you when it is done. There should now be a file folder on your USB drive with a name ending in ".odi". Remove the USB drive from the HMI and insert it into your development PC.

NOTE: Keep the ODI folder and make a backup of it in a safe place. Having a backup of an HMI application could save weeks of downtime should an HMI fail.

Step 5: Open MachineShop Suite

Open MachineShop Suite on your development PC. You should see something similar to the image below when it starts up. Click Create a New MachineShop Project. If you do not see this dialog box, you can also create a new project by clicking File > New Project. Give your new project a name and click OK.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Step 6: Add an HMI

In the upper right-hand corner of the screen, there should be an icon labeled EPX/HPX/IPX PowerStation that looks like an HMI. Click and drag that icon into the main project workspace next to the icon that looks like three gears. When prompted, give the device a name and click Next.

IMAGE BROKEN -- DCLIFFE

Step 7: Set up the Connection

You should now see the Connections dialog box. Click Add. Then, give your connection a name, set the type to Disk, and click Configure.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

You will then be asked what path you would like to use. Click Browse and navigate to the folder on the USB drive where you stored your ODI folder. Click OK.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

At this point, you will be returned to the Connections dialog box and will see your new connection in the selection box. Click Finish.

Step 8: Upload from Runtime

We are now ready to upload the application. In your project workspace, double-click the HMI that you dragged onto the screen earlier. In the dialog box that appears, select Upload Applications from Runtime and click Next.

IMAGE BROKEN -- DCLIFFE

On the Connections dialog, click Next. Then, click Finish. You will be prompted to overwrite existing applications (click OK) and may then need to select the application to upload if there are multiple applications on the disk. If this is the case, select an ODI folder and click OK. MachineShop Suite will verify that the upload was successful. You should now see the application at the bottom of your Project Browser on the left and can open and edit it by double-clicking it.

NOTE: This is a good time to save the project so that you have a backup copy. Click File > Backup Project to save a backup copy.

NOTE: Users who are uploading an old application into a newer version of MachineShop Suite may be prompted to upgrade their application. It is important to create a backup of the application before upgrading it as the upgrade process is not reversable. An application that has been upgraded to a higher version of InteractX cannot run on an HMI running a lower version of InteractX.

You now have an InteractX application that you can edit or deploy onto another HMI.

Transferring an Application from the Development PC to the HMI

Now that you already have a Disk Connection set up for this application (see Step 7 in the previous procedure), deploying your application to an HMI is a simple process that is essentially a reversal of the previous one. The steps are given below.

Step 1: Download to Runtime

Double-click the HMI object in your Project Workspace and select Download to Runtime. Click Next.

IMAGE BROKEN -- DCLIFFE

Select the connection you used to upload the application, then click Next.

IMAGE BROKEN -- DCLIFFE

Check the box labeled Application Files. Do not check the box labeled InteractX Runtime or the box labeled SQL Express (for Quick Logging). Click Finish. The application will download to the USB drive and MachineShop Suite will tell you when the process is complete.

IMAGE BROKEN -- DCLIFFE

Step 2: Download from Disk

Insert the USB drive into your HMI. Right-click on the Deployment Server icon in the bottom right-hand corner of your HMI's desktop and select Download from Disk in the option box that appears.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Click Browse and navigate to the location on the USB drive where you stored the ODI folder. Click OK and then click Finish. You will be required to select which ODI folder to use if you have more than one of them. In this case, use the dialog box that appears to navigate into the ODI folder and select the ODI file. Then, click OK.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Step 3: Finishing

After the download finishes, two dialog boxes will appear. The first one asks if you want to delete the ODI folder on the USB drive. Click No. The second one asks if you want to launch InteractX. Answer Yes or No as you see fit. If you choose No you can launch InteractX later by double-clicking the Deployment Server icon and clicking the Launch InteractX button.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

19JAN2017 DC

UPDATED 23JAN2017 DC: ADDED TRANSFER TO HMI SECTION AND CHANGED SOME WORDING

-->