Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Misc - Uploading and downloading InteractX projects over Ethernet
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Misc - Uploading and downloading InteractX projects over Ethernet
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX Upgrades
      • InteractX Misc - How to re-register older versions of Interact X (versions 1.x through 3.4)
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
InteractX Misc - Uploading and downloading InteractX projects over Ethernet

Print Friendly and PDF

There are three ways to transfer an InteractX application to or from an industrial PC running an InteractX runtime: disk (USB drive), Ethernet and serial. This FAQ will cover Ethernet, which is useful for frequent users of InteractX who need to deploy an application remotely or without opening a control cabinet. This procedure applies to the following Parker (CTC) HMI model lines:

  • PX
  • HPX
  • EPX
  • EPX2
  • IPX
  • IXA

For this method, you will need a laptop/desktop with MachineShop Suite installed on it. While uploading and downloading applications does not require a license, you will need one if you intend to do any editing of the application.

[Related FAQ: Uploading and downloading InteractX projects with a USB drive]

Transferring an Application from the HMI to the Development PC

This method will allow you to deploy or retrieve your InteractX application over a network without being physically near the HMI. It can also be help developers avoid additional labor and hassle during their design/test cycle. For this to work, your HMI will need to be connected by Ethernet back to your PC. This can be done using a variety of network topologies. The simplest connection is one from the HMI directly to your PC. Different topologies are described in brief below.

IMAGE BROKEN -- DCLIFFE
One Ethernet cable between the HMI and the development PC is the simplest network topology and the easiest one for a newcomer to set up.
IMAGE BROKEN -- DCLIFFE
A slightly more complex topology is one with a switch between the HMI and the development PC. This one is still easy to use, but it should be noted that the switch is a possible point of failure.
IMAGE BROKEN -- DCLIFFE
It is possible to deploy InteractX applications over a corporate network from a development PC to a plant floor HMI; many customers do this. This brings the additional complication that the two units must both have access to the network and be properly configured to see each other. If you want to deploy InteractX applications in this way, speak with your IT department early on so that the HMI can be given appropriate rights on the network.
IMAGE BROKEN -- DCLIFFE
Deploying InteractX applications over the Internet is unreliable and risky. Connection issues over the Internet can easily cause download failures and the download process opens an unprotected security hole in the network through which the download occurs. As such, this method is not supported. Users who need to do remote maintenance on InteractX HMIs are advised to run a remote desktop viewer and remote in a local development PC.

Step 1: Open MachineShop Suite

Open MachineShop Suite on your development PC. You should see something similar to the image below when it starts up. Click Create a New MachineShop Project. If you do not see this dialog box, you can also create a new project by clicking File > New Project. Give your new project a name and click OK.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Step 2: Add an HMI

In the upper right-hand corner of the screen, there should be an icon labeled EPX/HPX/IPX PowerStation that looks like an HMI. Click and drag that icon into the main project workspace next to the icon that looks like three gears. When prompted, give the device a name and click Next.

IMAGE BROKEN -- DCLIFFE

Step 3: Set up the Connection

You should now see the Connections dialog box. Click Add. Then, give your connection a name, set the type to Networks, and click Configure.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

Select Define runtime system now and click Details.

IMAGE BROKEN -- DCLIFFE

You can choose to define the connection based on the IP address of the InteractX HMI or its name. If your HMI has a static IP address, you can use it to set up the connection. This is usually best when the network is small and only consists of a few devices. If you are transferring an application over a company network with dynamic IP address assignment, you may want to set up the connection based on the PC name. After entering either an IP address or a PC name, click OK.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

InteractX supports the use of a username and password for upload and download access. If your InteractX HMI has a username and password configured for it, enter them in here. If it does not have a username and password, check Login Anonymous (click here if you are not sure). After that, click Finish.

IMAGE BROKEN -- DCLIFFEIMAGE BROKEN -- DCLIFFE

NOTE: The default setting on the HMI is Login Anonymous.

Step 4: Upload from Runtime

We are now ready to upload the application. In your project workspace, double-click the HMI that you dragged onto the screen earlier. In the dialog box that appears, select Upload Applications from Runtime and click Next.

IMAGE BROKEN -- DCLIFFE

On the Connections dialog, click Next. Then, click Finish. You will be prompted to overwrite existing applications; click OK. MachineShop Suite will verify that the upload was successful. You should now see the application at the bottom of your Project Browser on the left and can open and edit it by double-clicking it.

NOTE: This is a good time to save the project so that you have a backup copy. Click File > Backup Project to save a backup copy.

NOTE: Users who are uploading an old application into a newer version of MachineShop Suite may be prompted to upgrade their application. It is important to create a backup of the application before upgrading it as the upgrade process is not reversable. An application that has been upgraded to a higher version of InteractX cannot run on an HMI running a lower version of InteractX.

You now have an InteractX application that you can edit or deploy onto another HMI.

Transferring an Application from the Development PC to the HMI

Now that you already have a Disk Connection set up for this application (see Step 3 in the previous procedure), deploying your application to an HMI is a simple process that is essentially a reversal of the previous one. The steps are given below.

Step 1: Download to Runtime

Double-click the HMI object in your Project Workspace and select Download to Runtime. Click Next.

IMAGE BROKEN -- DCLIFFE

Select the connection you used to upload the application, then click Next.

IMAGE BROKEN -- DCLIFFE

Check the box labeled Application Files. Do not check the box labeled InteractX Runtime or the box labeled SQL Express (for Quick Logging). Click Finish. The application will download to the HMI and MachineShop Suite will tell you when the process is complete.

IMAGE BROKEN -- DCLIFFE

NOTE: If you have also read the FAQ about downloading applications using a USB stick, then you have probably realized that downloading over Ethernet has fewer steps. Because of this, we recommend that regular users of InteractX use the Ethernet download utiliy as it will save them time.

 

Tips and Tricks

There are things to keep in mind when performing upload and download operations over Ethernet. A few of them are summarized below, but this list is not comprehensive, especially for corporate networks.

  • For a download to work, the Deployment Server must be running on the HMI.

  • InteractX will not allow you to transfer an application if your username and password are incorrect or if your unit does not allow anonymous login. You can change the username and password (or remove it) on the HMI using the Deployment Server. On your HMI's desktop, click or right-click the bowling ball icon in the taskbar. In the option panel that appears, click Network. Here, you can set the username and password.

  • If you cannot get to the Deployment Server because your HMI is running an InteractX application, try the following:

    • Press an Exit button in the application.
    • On a keyboard, press Alt+F4.
    • On keyboard, press Ctrl+Alt+Delete. From there, open Task Manager and kill the HMIRun.exe process.

    If none of the above options work, call 707-584-7558 or email emn.service@support.parker.com

  • If you are connecting using a static IP address and it is not working, try sending a ping command to see if that address is reachable from your PC. If it is not, you may have an IP address or a subnet mask configured improperly.

  • PCs that have Gigabit LAN ports can typically use either crossover or straight-through Ethernet cables when communicating with any other device. This is because the Gigabit standard requires crossover auto-detection. However, older PCs may only support 100 BASE-T and may not offer auto-detection. You can always check to see if the physical connection is good by looking at the lights on the Ethernet port. If they are on or blinking, the electrical connection is fine. If they are not, try using a different cable or adding an Ethernet switch to the system.

23JAN2017 DC

Fixed link 30NOV2017 DC

-->