Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress-
      • Interact Xpress Misc - How to Flashback Compact Flash (CF) Card for Parker HMIs
      • Flash Player - Parker Remote Browser compatibility issues with the older versions of Xpress
      • Interact Xpress C3 Error History Display
      • INTERACT XPRESS HOW TO ORDER
      • Interact Xpress Manager - Troubleshooting - Ver 4.2 Error Flash Player not installed
      • Interact Xpress Misc - Are all tags written all the time? Where to set this?
      • Interact Xpress Misc - Can I send an Alarm E-mail to more than one person?
      • Interact Xpress Misc - Creating New Projects for older versions of Xpress using Seed Projects in Xpress Manager 4.x
      • Interact Xpress Misc - How can I find out what TCP/UDP ports my software is using?
      • Interact Xpress Misc - How do I get through my router for remote Interact Xpress panel access?
      • Interact Xpress Misc - How to change the sort order for recipes in Xpress?
      • Interact Xpress Misc - Loading Xpress Application on the XPR on bootup
      • Interact Xpress Misc - Test PLC driver connection setup BEFORE downloading to the HMI - If the Development PC can not talk to PLC, the HMI won't ether.
      • Interact Xpress Misc - Updating the Firmware (Xpress version) on the Xpress HMI Hardware
      • Interact Xpress Misc - Updating Xpress Project Versions & Creating Backup Copy
      • Interact Xpress Misc - User Configurable Driver User Guide (UCON)
      • Interact Xpress Misc - What can I do if I don't know the Xpress Admin Password?
      • Interact Xpress Misc - What size Compact Flash card is supported by XPR/XPC?
      • Interact Xpress Misc - Where is the driver documentation and tag format information?
      • Interact Xpress Misc - Which HMI runs Interact Xpress?
      • Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
      • Interact Xpress Misc - XPC2, XPR2 and EPX2 PowerStations no longer include audio hardware (SB975)
      • Interact Xpress Misc - XPR/XPR2 Flashback Utilities
      • Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
      • Interact Xpress Misc - Xpress Flashback for XTA and required Memory Card.
      • Interact Xpress Misc - Xpress Manager Archive
      • Interact Xpress Misc - Xpress Time and Date Tags and how they are related and used to set the HMI system Time and Date
      • Interact Xpress Software - Control Access to Panels and Tools using the Password User Levels in Xpress / Embedded Xpress (PAC)
      • Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
      • Interact Xpress Software - How do I set a value to my device from my Xpress panel only when a button is pressed?
      • Interact Xpress Software - How do I write/read strings between Xpress (XPR) and ACR?
      • Interact Xpress Software - How to switch screens from a PLC
      • Interact Xpress Software - How to wrap text on a tool in Xpress Manager?
      • Interact Xpress Software - Xpress Recipe Naming
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Controller (Global) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Program (Local) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Driver - Manual Creation of Controller (Global) STRING Tags in Xpress Manager
      • INTERACT XPRESS TRAINING - AB CONTROLLOGIX ETHERNET DRIVER - MANUAL CREATION OF PROGRAM (LOCAL) STRING TAGS IN XPRESS MANAGER
      • Interact Xpress Training - Importing Tags into Xpress from Control Logix / Compact Logix
      • Interact Xpress Training - Interact Xpress with Parker-SSD AC890 Drive Products
      • Interact Xpress Training - Tag Rules (Tag Sharing) Examples
      • Interact Xpress Training - Using with Compax3 for Torque Control (Example)
      • Interact Xpress Troubleshooting - Auto E-Mail on Alarm activity not working with Free E-mail servers
      • Interact Xpress Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Interact Xpress Troubleshooting - Fonts unreadable on tools or animations broken after upgrading 2.16 and older Projects to 3.1 or 4.1
      • Interact Xpress Troubleshooting - If losing connection to PLC, turn on Auto-Demotion
      • Interact Xpress Troubleshooting - Messages disappear from Multi-State indicator after application closed and re-opened when & is used in message
      • Interact Xpress Troubleshooting - My Xpress projects disappeared after I upgraded my Pre-2.1.6 version to 2.1.6 or higher
      • Interact Xpress Troubleshooting - My Xpress version did not change when I did an upgrade to the latest version on my development PC
      • Interact Xpress Troubleshooting - Not able to add tags in Tag Editor using (New Tag)
      • Interact Xpress Troubleshooting - Step 3 Error when clicking Design in your Xpress Project
      • Interact Xpress Troubleshooting - UCON Floating point values have Commas where the Decimal point should be
      • Interact Xpress Troubleshooting - Workaround for getting flash to work on Android 4.0xxx revs
      • Interact Xpress Troubleshooting - XPR / XPR2 Flash Player error dialog pop-up (long running script....) or screen stops updating.
      • Interact Xpress Troubleshooting - Xpress Manager / Unable to Exit Runtime or Designer running on Windows 10
      • Interact Xpress Troubleshooting - Xpress Manager crashes when importing a JPG
      • Interact Xpress Troubleshooting - Xpress Manager Menus clipped/chopped off. Setting size to Small/Medium/Large does not change the viewable menu.
      • Interact Xpress Troubleshooting - XT replacement panel won't connect over ethernet
      • Parker Remote Browser -- Connect to Xpress HMI at Startup
      • Xpress 4.2 install OCX failed to register and the Xpress Manager "Help - About IXM " shows blank Flash player version.
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?

Print Friendly and PDF

The Lens States in the Indicator tool are controlled by the three fields: Lens Output1, Lens Output2, and Lens Output3 (these are located under the Values property for the indicator tool).

These three fields provide a binary pattern that corresponds to a particular Lens State with Lens Output1 being the LSB and Lens Output3 being the MSB.

For example, if the fields evaluate as Lens Output1 = True, Lens Output2 = False, Lens Output3 = True, this corresponds to the binary pattern 101 which equates to 5 and thus Lens State 5 will be the active one.

So, how do I control the Lens state with a numeric value 0 through 7 then?  This simply requires a little logic added to each field.  If my tag is called "TagName" then:

The Value for Lens Output1 would be:    TagName & 1

The Value for Lens Output2 would be:   TagName & 2

The Value for Lens Output3 would be:  TagName & 4

This will apply a bitwise AND function between the tag value and the bit we care about for each field.  So if my TagName contained the value of 5, the above logic would provide the TRUE, FALSE, TRUE pattern we want (101) and thus Lens State 5 would be active. 

Note - you can edit the appearance of each Lens state under the Appearance section of the Indicator properties.

glh  4/2017