Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Common PACIO Troubleshooting Tips
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Common PACIO Troubleshooting Tips
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
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
      • Electromechanical – Mobile Forums
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
Common PACIO Troubleshooting Tips

Print Friendly and PDF

The following topics are common installation and/or configuration related problems that customers may encounter as well as a description of the symptoms.

1.  Some modules require an additional 24VDC supply connection. 

If the module has L+ and L- terminals (will also have a status LED labeled as Power) it requires this additional 24VDC connection (see PAC user guide for reference).  If this additional 24VDC connection is not provided, the input, output or channel variables will not update when scanned by the PAC. 

The Power LED on the module will be off as an indicator that this is the problem.  Some modules may also show an Undervoltage fault (analog modules) if you are getting some variable updates.

The modules will come on-line on the EtherCAT bus since the bus derives its power from the controller but you will not get variable updates of the actual physical circuits (inputs, outputs, channels).

************************************

2.  PACIO module order in your PAC project bus must be the same as the physical order of the modules on the bus.  If the order in the project is different from the physical order on the bus then the EtherCAT bus will not start running after you start the PLC.  You will see the red triangle symbol by each of the devices on the bus (see picture). 

This is also true of other devices that may be on the EtherCAT bus as well.

************************************

3.  This final tip isn't something mis-installed or mis-configured.  Instead, it is a default setting in your project for each device that won't update I/O unless they have been mapped to variables and are being used in a POU and thus being scanned in a task. 

However, it's often useful to verify your physical connections before you have proceeded with much of your variable mapping and programming.  So, there are some settings you can change that will allow the I/O and variables to update even if you don't have POUs yet.

The simplest place to change this is in the PAC320 Device properties itself.  Double click on the PAC320 device in the project tree and select the PLC Settings tab.  The checkbox "Update IO while in stop" will allow the PAC to start the EtherCAT bus (but not any soft motion axes) once you go on-line without starting the PLC.  The second setting to change is the "Always update variables".  Change this to "Enabled 2 (always in bus cycle task)". 

Now when you go on-line it will start the EtherCAT bus and update the I/O for all of the modules under their EtherCAT I/O Mapping tab.  You can also force outputs from this screen.

If you don't select the "Update IO while in stop" option you can still select the "Enabled 2 (always in bus cycle task)" option.  Then you will have to start the PLC for the I/O to update but you don't need the I/O mapped to variables yet with this setting.

Each device itself (PACIO or drives, etc.) will also have a setting similar to this for that particular device (as opposed to all of them updating).  This will be in the lower right corner of that device's EtherCAT I/O Mapping tab.  The default setting is "Use parent device setting" which is then dependent on the PAC PLC Settings mentioned earlier.  If you change this to "Enabled 2 (always in bus cycle task)" then this specific device's I/O will update when the PLC is running regardless of that similar setting under the PAC itself.  Useful if you just want to troubleshoot a specific module after installing it.

glh 5/2017

PACIO fault PACIO error PACIO issue PACIO mistake PACIO problem