Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)

Print Friendly and PDF

  The 63x family has been discontinued and system upgrades will be required.

The Parker (SSD / Eurotherm) servo drive 630 family includes the 631, 635, 637, 637F, and 638 designs.  These are European drives that are not catalog items for the EM&D division.

The modern Compax3 family is the primary option for system upgrades and some re-engineering will be required.  It is not a drop-in replacement.  The overall system requirements will need to be understood to know which version of the Compax3 family will be the best option.  The IPA and P series servo drives may also be options depending on the system requirements and motor being used.  Configuration and programming changes will be required as well as installation and cabling changes. If you require assistance with redesign, a local Parker Distributor in your area can assist as well.

****************************************************

Older information for reference only:

The 637F and 638 may be possible replacement options sold through the EM&D custom product system, though the EM&D support will be limited.  The 637F/638 had higher position resolution so some programming and parameter adjustments will be necessary.  The 638 also uses different motor and power supply connectors and includes an additional STO connector.

Here is some useful comparisons and user documentation:

For 631 / 635 replacements, the 638A was the closest replacement.

631/635 Replacement

For the 637, the 637F or the 638B are the closest replacements.  They each have different position resolution resolutions requiring programming / parameter changes.  The 638B also used different motor and power connectors and includes an additional STO connector but is a new option.

This compares the 637F and 638B specifications:

637F versus 638B

User Guides:

635

637

637+

637F

638

Note - the 635 may also be known as the APOLLO drive (ASB, Germany)

Note - the 637 may also be known as the SAMSON drive (ASB, Germany)

  

glh  6/2017

glh 5/2018 update

13SEP19 Update

  • 630
  • 637
  • 635
  • 637F
  • Parvex
  • 638
  • 631