Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Using a PHM monitor with a headless XPR/XPR2 unit
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Using a PHM monitor with a headless XPR/XPR2 unit
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)-
      • Is there a Windows7 / Windows 10 driver for my PHM / PM1 touchscreen interface?
      • Using a PHM monitor with a headless XPR/XPR2 unit
      • What can replace a PM1 or PHM industrial touchscreen monitor?
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Using a PHM monitor with a headless XPR/XPR2 unit

Print Friendly and PDF

The PHM touchscreen monitor can be used with the headless XPR or XPR2 units as its display and touchscreen.  However, the XPR/XPR2 unit must be configured for this combination first (out of the box it will not be).

Remove the Compact Flash card from the XPR/XPR2 unit and run the flash back utility (see link to Flash Back Archives below).  Find the version that you are using and run the utility in the XRPT&XPR2T folder.  This is the version for use with the PHM external touchscreen. 

Flashback Archives

Now transfer your application back to the CF card.  Plug in a VGA cable between the XPR/XPR2 headless unit and the PHM and an RS232 cross over (null modem) cable between the PHM and the COM1 port on the XPR/XPR2 unit. 

 

 

glh   6/2017

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply