Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Vix-IE with Brushed motor and Encoder
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Vix-IE with Brushed motor and Encoder
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Vix-IE with Brushed motor and Encoder

Print Friendly and PDF

When running a ViX-IE drive with a brushed motor that also has encoder feedback, it is necessary to have LOADENC set to 1 and the following wiring configuration for the X2 and X4 connectors.


Connection on the Vix X1 connector
Vix X1 connector Motor Terminal
Motor phase U +
Motor phase W -



Connection on the ViX X2 connector
HALL 1 (pin 9) and 2 (pin 13) are jumpered to GND



Connection on the Vix X4 connector
Vix X4 Pin Encoder Signal
4 GND
5 +Vcc (+5VDC)
7 /A
8 B
12 A
13 /B


Notes on LOADENC

The default setting for LOADENC is 0, which sets the Vix drive to commutate from the X2 encoder input. The current output on phase U and W will vary based on the position of the encoder connected to X2. 

With LOADENC set to 1, the Vix drive does not servo from the X2 encoder input, but will instead servo from the X4 encoder input. The current output will be determined by the Hall signal input on the X2 connector, in this case for the U and W phase outputs. 

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply