Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Winding Tolerances and Resistance Measurement
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Winding Tolerances and Resistance Measurement
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
  • AC/DC Industrial Drives+
  • Gearheads+
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners-
    • IForce Linear Servo Motors & Positioners-
      • When should I used a linear motor stage?
      • What are the main precision application types for linear motor stages?
      • Can Parker provide custom linear motor stage solutions?
      • 110 WD0 Motor Specifications
      • 310 Coil Bar Side Mounting Locations
      • Air Cooling and Liquid Cooling Notes
      • Can I use the motor in vertical applications?
      • Current Derate for less <0.5pitch moves
      • D Dual parallel winding specs
      • Different types of linear motors
      • Do the magnets lose their magnetism with time?
      • Does the motor coil float between the magnets?
      • Hall-Effect, Home and Limit Module Wiring
      • High Pot Option
      • How do I select a linear motor?
      • How to Wire MHED Limit/Home/Halls Module
      • IForce Coil Compatibility in Vacuum Environments
      • Importance of mechanical alignment
      • Inspection Report
      • LEM Feedback Troubleshooting & Replacements
      • LME vs PLME Linear Magnetic Encoders
      • ML18 Track Weights
      • Motors used underwater or in the presence of oils
      • No motors listed in WinTips motor database?
      • Old IForce actuator part numbering
      • Omega 44004 Thermistor Info
      • Parker MotionSizer - Temperature Rise Calculation
      • Phasing Diagram
      • Renishaw Optical Encoders
      • Trilogy Electrical Pitches
      • Trilogy Extension Cables
      • Trilogy High Flex Cable Specifications
      • Trilogy IForce Cooling Options
      • Trilogy IForce Custom High Vacuum Options
      • Trilogy Motor Summary & Drive Compatibility
      • Trilogy Motors with Non-Parker Servo Drives
      • What are the minimum bend radii of Trilogy THF flex cables?
      • What voltage for IForce hall-effect sensors?
      • Which MHED is used within the positioners?
      • Why do some motors have steel laminations?
      • Why lamination designs skew or angle their magnets
      • Winding Tolerances and Resistance Measurement
    • MX80+
    • mSR+
    • Ripped Series Linear Motors & Positioners+
    • LXR+
    • mPR+
    • XE+
    • XR+
    • ZP Wedge+
    • P8S Position Sensor order codes
    • How can I know if a given actuator is suitable for use in a specific environment?
    • Manufacturer Grease Standardization
    • I need speed and accuracy over a long length. What type of actuator should I use?
    • What type of encoder options are available for the Trilogy Series?
    • What type of material is used for the base of the Trilogy Linear Motor Positioners?
    • LBB / LBZ / LBN Linear Actuator Model Numbers
    • Parker Limit and Home Sensor Compatibility
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
Winding Tolerances and Resistance Measurement

Print Friendly and PDF
The Trilogy coils' winding tolerance is a standard +/-10% for the resistance and within .5 ohms between each of the phases and +/-30% for the inductance, similar to rotary servo motor tolerances. The magnet tracks can see a variation in magnet strengths of 3-5% from one manufactured lot to the next. All magnets will meet the minimal magnet specification. Normally, their strength exceeds the minimum.

Please note that the I-Force catalog resistance specifications are for the motor in delta wiring. If checking the resistance of a motor with six-lead option (110, 210 or 310 motor with WD1 or WD2 wiring options) with an ohm-meter, the third phase will need to be tied together in order to measure the correct resistance across the first two phases.

For example, for a 310-4 with WD2S wiring, measuring the resistance between red&blue (A) and black&brown (C) will be 17.2ohms +/-10% with the green&white (B) tied together. Without the green&white (B) the measured resistance will be the individual phase resistance which is 1.5 times the cataloged delta resistance, in this case 25.8ohms +/-10%.

All other motors and wiring options have the 3 motor leads (red, brown, orange) and measuring the resistance across any two phases will match the catalog resistances.

Please note catalog specifications are for delta wound motors. Consult factory for WD0 wye wound motor specifications.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply