Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I set up Parker I/O (PIO)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I set up Parker I/O (PIO)
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)-
        • ACR9000 Family Letter of Volatility
        • ACR Gantry Lock and EPL Axes
        • ACR Homing Success/Failure Flags
        • ACR Order Code
        • ACR Servo Tuner - Move Back & Forth sample code
        • ACR-View 6 is frozen. How do I recover?
        • ACR-View Memory Dimensioning using the Oscilloscope
        • ACR9000 to ModuFlex connection pinout
        • Automating the EPL startup procedure
        • Can I use tools from ACR-View in my own PC application?
        • Compax3 and Aries Ethernet PowerLink I/O
        • Configuring Memory for ACR9000 Com Channels
        • Dual Loop with Analog Position Feedback
        • EPL Drive Enable Status
        • Free Online Training Videos: Parker ACR9000 programmable motion controller
        • Having problems connecting with USB - ACR View 6.0
        • How do I add PBOOT to PLC programs?
        • How much memory does my ACR controller have?
        • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
        • How to Read Compax3 Analog I/O with EPL SDO read?
        • How to connect ACR to PIO CANopen buscoupler?
        • How to disable RS232 autobaud for ACR9xxx
        • How to get status values from an Aries EPL Drive
        • How to read the absolute position from EPL drive?
        • How to select user units and axis scaling
        • INTCAP and MSEEK with Compax3 EPL
        • MSEEK EthernetPowerlink Compatibility
        • Memory Allocation for PLC programs
        • Output Reaction to EPL Failure
        • Remap CAN I/O for use with PLC
        • What is needed with various Parker I/Os?
        • What verison of the .Net Framework is needed for ACR-View 6?
        • Whats the difference between PIO-337 and PIO-347?
        • Where does ACR-View install the ComACRserver?
        • Why is controller reporting Program Stuck
        • 9000: Connector Part Numbers
        • ACR 9000 replacement: New ACR7000 series controller
        • ACR 9xx0 Recovering from Estop / Motion Enable input
        • ACR-View: Mapping a parameter to an oscilloscope channel
        • ACR9000 - CIP Communications stop on all devices when one CIP device goes offline
        • ACR9000 Ethernet Stream Connection Status Sample
        • ACR9000 Event Counters
        • ACR9000 Sample Input/Output Wiring
        • Are Parker IO modules available as NPN?
        • Connecting a Parker IO (PIO) to an ACR9000
        • EPL Velocity p38145 vs p8193 Master Velocity
        • Ethernet Communication Streams
        • Ethernet/IP Encoders
        • How do I set up Parker I/O (PIO)
        • How to command a home operation from HMI or PC app
        • Master Encoder for C3 EPL & ACR9040 system
        • Maximum USB Cable Length
        • Replacing the ACR9000 Battery
        • RS232 Electrical Noise on older 9000 Controllers
        • Senary Axis Flags
        • Updated EPL Network Flags and Parameters
        • Upload Absolute Position from a C3 to a ACR9000
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
How do I set up Parker I/O (PIO)

Print Friendly and PDF

What is Parker I/O and how do I set it up? 

Parker I/0 is a CAN based product which allows some Parker products to expand I/0 capability for digital inputs, outputs, analog inputs and analog outputs. The Parker I/0 module can be configured using dipswitches that are built into the coupler module. The coupler module controls the communicate speeds and node ID.

The following steps are required to setup the baud rate and node ID on the coupler...

To set the baud rate:
Step 1. Turn off all switches.

Step 2. Power on the coupler.

Step 3. Adjust the baud rate according to table below.

Step 4. Set switch # 8 to on.

Step 5. Switch off the coupler.
<width="100">

SWITCH Function 1MBIT 800KB 500KB 250KB 125KB 100KB 50KB 20KB 10KB Indicated by LEDS
1 (LSB) Baudrate 0 1 0 1 0 1 0 1 0 STOP
2 Baudrate 0 0 1 1 0 0 1 1 0 RUN
3 Baudrate 0 0 0 0 1 1 1 1 0 TX-Overflow
4 (MSB) Baudrate 0 0 0 0 0 0 0 0 1 RX-Overflow
5



To set the node id:
Step 6. Make sure the coupler is off.

Step 7. Adjust node id by setting appropriate switches

Step 8. Turn on coupler

For software configuration and to start network communication please see your specific product manual.
ACR 9000 Setup
In the Configuration Wizard, under CANOpen Master Setup, do the following:

1. In the Master Node ID box, select the address you want to assign the controller.

2. In the Bit Rate (kbps) box, select the bit rate used in the network.

3. In the Cyclic Period (ms) box, enter the cyclic period for the network.

4. Under CANOpen Slave Setup, do the following:

5. In the Number of Slave Nodes box, select the number of nodes in the network.

6. For each slave node, select the address you want to assign.

7. Click on "Start CANopen Network"

PLEASE NOTE! You do not need to change the master setup. The only setup required is to match your hardware coupler to the default slave settings.

Related FAQs: Connecting a Parker IO (PIO) to an ACR9000

Expansion IO (PIO) with Compax3

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply