Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base AT6000 Product Issues
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base AT6000 Product Issues
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
  • AC/DC Industrial Drives+
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000-
      • 6000 Servo Products I/O Updates
      • 6000 Step Products Analog Inputs
      • 6250 Analog Input Option (-ANI)
      • 6250 and AT6250 Third Encoder Port
      • AT Servo Cards & Windows NT - OS Lock-Up
      • AT6000 Auxiliary Cables
      • AT6000 Product Issues
      • AT6200 and AT6400 are now CE marked
      • AT6XXX
      • AT6xxx Operating System Compatibility
      • AT6xxx Operating System Files
      • Auto-load operating system at startup
      • Backing up 6000 Programs
      • Bad DLL Calling Convention
      • Control Velocity with an Analog Input.
      • DDE 6000 and Excel
      • Downloading Programs in a Daisy Chain
      • Home Backup Controls Cluster with Motion Toolbox
      • Homing to Z channel on 6000 products
      • HOMLVL command
      • How do I change velocity on the fly during JOGGING?
      • How do I make a program run on power up?
      • How do I make a proper back up for my 6000 series controller?
      • How to send/receive with OCX
      • Input Buffer for 6000 Serial Producs
      • Input Debounce Times for 6000 Series Products
      • Input Impedance for -ANI option for AT6n50
      • Interrupts, AT cards & troubleshooting
      • Linker Error
      • LSCW and LSPOS are the same command
      • Minimum files for AT card
      • Model 6201 Information
      • Motion Architect and WinRT
      • Motion Toolbox in a Daisy Chain
      • PCOMP in Conditional Statements
      • Reading in multiple numbers with the TM8
      • ReceiveFile method bug
      • RecvAT6400Block documentation error
      • Running more than 199 programs in 6000 Products
      • Scaling With the 6000 Products
      • Sequence Names Can Cause Problems.
      • SetNTMultiCardAddress doc error
      • Status Bits and Commanding a Velocity of Zero
      • Unable to get Procaddress32W for wrtoutpw error
      • VIDEO: DDE Server - Communicating from MS-Excel
      • Visual Basic Sample with AT Card
      • What addresses are in use on my NT machine?
      • What can I use as a replacement for my 6200 or OEM6200 indexer?
      • What can I use as a replacement for my 6250 or OEM6250 servo controller?
      • What can I use as a replacement for my AT6200 or AT6400 indexer?
      • What can I use as a replacement for my AT6250 or AT6450 servo controller?
      • What is WinRT anyway?
      • Why does RESET6000.VI cause error 5004 in Labview?
      • Why is my AT-card locking up?
      • Why is the motor not moving when I command it to?
      • X language to 6000 series language
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637, 638) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
AT6000 Product Issues

Print Friendly and PDF

Compumotor Applications Engineering Department is aware of two issues regarding the AT6000 products that may be causing some confusion in the field. The purpose of this Technical Bulletin is to attempt to clarify these issues for current and potential users of these products.

AT6n00/OEMAT6400 and AT6n50 Memory (RAM) Specifications and Implications 
Before August 1997, AT6000 products had expanded memory available as an option. Since August 1997, all products have been shipping with expanded memory as a standard feature. This change is referenced in Sales Bulletin 417 (August 22, 1997) but the memory specifications given in that bulletin are incorrect. The correct memory specifications are provided in the current Compumotor Catalog (Catalog 8000-2/USA) and are as follows:

AT6200/AT6400 and OEMAT6400 1.5 Mbytes RAM
AT6250/AT6450 150 Kbytes RAM


This memory expansion could have a minor consequence on applications. With expanded memory, it now takes longer (approximately 2 seconds longer) to initialize the AT6000 after the operating system file has been downloaded. Users should delay at least this long before trying to query or send commands to the AT6000 controller.
Computer Companies Eliminating Full-Length ISA Slots in Some Models 
It has come to our attention that some computer manufacturers are not including full-length ISA slots in some models. For example, Compaq only offers a full-length ISA slot in their tower version. Apparently, this is a trend that will continue with almost all PC manufacturers. This development was precipitated from the fact that sound and modem card manufacturers have completely changed over to half-length cards.

When specifying a computer for use with an AT6000 product, it is important to verify that the computer has a full-length ISA slot available. This is also true for other motion control companies that offer full-length ISA motion cards.

Compumotor next-generation 6000 products will offer an alternative pc-connectivity, such as Ethernet, Profibus, Fieldbus, and SERCOS. Contact the Applications Dept. for more details.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply