Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How do I make a proper back up for my 6000 series controller?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How do I make a proper back up for my 6000 series controller?
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000-
      • 6000 Servo Products I/O Updates
      • 6000 Step Products Analog Inputs
      • 6250 Analog Input Option (-ANI)
      • 6250 and AT6250 Third Encoder Port
      • AT Servo Cards & Windows NT - OS Lock-Up
      • AT6000 Auxiliary Cables
      • AT6000 Product Issues
      • AT6200 and AT6400 are now CE marked
      • AT6XXX
      • AT6xxx Operating System Compatibility
      • AT6xxx Operating System Files
      • Auto-load operating system at startup
      • Backing up 6000 Programs
      • Bad DLL Calling Convention
      • Control Velocity with an Analog Input.
      • DDE 6000 and Excel
      • Downloading Programs in a Daisy Chain
      • Home Backup Controls Cluster with Motion Toolbox
      • Homing to Z channel on 6000 products
      • HOMLVL command
      • How do I change velocity on the fly during JOGGING?
      • How do I make a program run on power up?
      • How do I make a proper back up for my 6000 series controller?
      • How to send/receive with OCX
      • Input Buffer for 6000 Serial Producs
      • Input Debounce Times for 6000 Series Products
      • Input Impedance for -ANI option for AT6n50
      • Interrupts, AT cards & troubleshooting
      • Linker Error
      • LSCW and LSPOS are the same command
      • Minimum files for AT card
      • Model 6201 Information
      • Motion Architect and WinRT
      • Motion Toolbox in a Daisy Chain
      • PCOMP in Conditional Statements
      • Reading in multiple numbers with the TM8
      • ReceiveFile method bug
      • RecvAT6400Block documentation error
      • Running more than 199 programs in 6000 Products
      • Scaling With the 6000 Products
      • Sequence Names Can Cause Problems.
      • SetNTMultiCardAddress doc error
      • Status Bits and Commanding a Velocity of Zero
      • Unable to get Procaddress32W for wrtoutpw error
      • VIDEO: DDE Server - Communicating from MS-Excel
      • Visual Basic Sample with AT Card
      • What addresses are in use on my NT machine?
      • What can I use as a replacement for my 6200 or OEM6200 indexer?
      • What can I use as a replacement for my 6250 or OEM6250 servo controller?
      • What can I use as a replacement for my AT6200 or AT6400 indexer?
      • What can I use as a replacement for my AT6250 or AT6450 servo controller?
      • What is WinRT anyway?
      • Why does RESET6000.VI cause error 5004 in Labview?
      • Why is my AT-card locking up?
      • Why is the motor not moving when I command it to?
      • X language to 6000 series language
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
How do I make a proper back up for my 6000 series controller?

Print Friendly and PDF

Here are the steps required to make a proper back up for a 6000 series controller.

1.Upload  the  programs from the working unit.
2. Go to the terminal Emulator. Issue the following commands and make note of the responses from the controller. If the controller is busy running a program, it will be necessary to insert an "!"  before each command (example: !SCALE).

SCALE
SCLD
SCLV
SCLA
SCLMAS
STARTP
3.Open up the uploaded file. It should look something like this:
DEL Setup     
DEF Setup   
...
END
4.Insert the four scaling commands above the first line of the uploaded code. It should look something like this:
SCALE 1               
SCLA 25000
SCLD 12500
SCLV 25000
SCLMAS 4000
DEL Setup
DEF Setup
...
END
Please note that this example is for a single axis controller. These are example values and you should use values that you uploaded from the old controller.
5. After the last END statement, insert the STARTP command. The last line of the uploaded code should be END It should look something like this:
END
STARTP Setup
Now save this file. You have successfully created a back up file for your controller.
Note: not all applications use SCLMAS; this is a scaling factor for the master and used in following/gearing applications. This affects FOLRN, etc and thus needs to be outside program like the other scaling parameters.
If scaling is not set the affect parameters such as D for distance will not be correct if you do a TPROG SETUP in the terminal (or other program -- see TDIR to see list of programs) and compare with the program editor.