Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base P Series Drives - How to Reset Single Turn Absolute Position to Zero (PM-DD example)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base P Series Drives - How to Reset Single Turn Absolute Position to Zero (PM-DD example)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series-
      • P Series Accessories - 50 Pin I/O Breakout Module Labels (APC-VSCN1T05)
      • P Series Accessories - AC Mains Filter (Noise Filter - RFY-4010M)
      • P Series Accessories - Brake Resistor Dimensions
      • P Series Accessories - Options and Drawings
      • P Series Cables - Bend Radius
      • P Series Cables - Encoder Cable Color Code and Specs
      • P Series Cables - High Flex Power and Feedback Cable Specifications
      • P Series Cables - Motor Power and Encoder Cables
      • P Series Cables - Multi-turn Feedback Cable Battery
      • P Series Drives - Analog Monitor (Output) Specs
      • P Series Drives - Brake Control
      • P Series Drives - Can single-turn encoder cables be converted to multi-turn cables in the field?
      • P Series Drives - End of Travel Limit Behavior
      • P Series Drives - EtherCAT Version - Safety Rating
      • P Series Drives - EtherCAT Version - STO bypass connector for the P Drive
      • P Series Drives - EtherCAT Version - STO Wiring
      • P Series Drives - Hall-less commutation
      • P Series Drives - How to Reset Single Turn Absolute Position to Zero (PM-DD example)
      • P Series Drives - How to Reset Drive's Internal Absolute Encoder Offset
      • P Series Drives - Indexer Version - How do I change the step (pulse) input resolution for the P Series in Pulse mode?
      • P Series Drives - Indexer Version - Analog Inputs (command inputs) for Torque Control (or Velocity Control)
      • P Series Drives - Indexer Version - Analog Mode or Step & Direction (Pulse) Mode Sample Configurations & Notes for ACR9000 and ACR7000 controllers
      • P Series Drives - Indexer Version - Cabling information to ACR9000 and ACR7000 controllers
      • P Series Drives - Indexer Version - Can I get absolute encoder position from my drive?+
      • P Series Drives - Indexer Version - Clarification of Velocity Command Switch Functionality
      • P Series Drives - Indexer Version - How to do Scaling
      • P Series Drives - Indexer Version - Interact Xpress Example Project File (Modbus/RTU)
      • P Series Drives - Indexer Version - InteractX Complete Modbus Addressing Example (Modbus/RTU)
      • P Series Drives - Indexer Version - ISELx pattern (Index Addressing Inputs)
      • P Series Drives - Indexer Version - Max Encoder Output Frequency
      • P Series Drives - Indexer Version - Modbus/RTU Addresses Incorrect in User Guide
      • P Series Drives - Indexer Version - Product Overview
      • P Series Drives - Indexer Version - RS-422 Pin-out
      • P Series Drives - Input Power, Output Current, Power Ratings, and Installation Diagram (L1/L2/L3 and C1/C2) - Includes Low Voltage Configuration and Wiring
      • P Series Drives - Installation Spacing and Cabinet Losses
      • P Series Drives - Limit and Home Wiring
      • P Series Drives - Motor and Power Connector Terminals
      • P Series Drives - Motor Files and Setup for MPP / BE / SM / J / N / mSR / mPR / LXR / 110 / 210 / 310 / 410 / T1 / T2 / T3 / T4 Motors (Incremental Encoders w/ Halls)
      • P Series Drives - MPP/MPJ servo motors with the BiSS-C encoder option (4B)
      • P Series Drives - Short Circuit Current Rating (SCCR)
      • P Series Drives - UL Listing
      • P Series Drives - What is N input pin next to L1, L2, L3?
      • P Series Misc - Bayside Direct Drive Rotary R100D, R150D, R200D replacements
      • P Series Misc - Dynaserv Replacements
      • P Series Motors - Brake Option Specifications, Wiring Diagrams, Configuration Parameters (for P Series Drives)
      • P Series Motors - Mechanical Tolerances
      • P Series Motors - Pole Counts
      • P Series Motors - Shaft Load Ratings
      • P Series Motors - Speed/Torque Curves 120/240vac (PM-Fxx)
      • P Series Motors - Temperature Protection
      • P Series Motors - Torque and Voltage Constants
      • P Series Software - Drive Support Tool Overview Video+
      • P Series Software - Drive Support Tool training and Auto-tuning
      • P Series Software - Firmware and Software Archive
      • P Series Troubleshooting - Alarms and Warnings
      • P Series Troubleshooting - What is W20 and how do I fix it?
      • P Series Troubleshooting - Drive does not enable but also does not report a fault
      • P Series Troubleshooting - Drive Support Tool connects via USB ok, but the Setup Wizard and/or Firmware Update tool are not able to
      • P Series Troubleshooting - Drive Support Tool USB communications / driver Windows 10 (WIN10) and 7 (WIN7)
      • P Series Troubleshooting - Indexer Version - Can Enable/Disable from Drive Support Tool PTP Screen but Cannot Jog/Move
      • P Series Troubleshooting - Modbus addressing for Index objects - Writes OK but getting bad data returned (Interact Xpress)
      • P Series Troubleshooting - My P Series Indexer only makes Index0 moves when under input control
      • P Series Troubleshooting - Why is my motor shaft rough? (dynamic braking setting)
      • P Series Drives - Indexer Drive Connector Part Number Incorrect in rev A of User Manual
      • P Series Drives - Indexer Version - Video Training: Overview & Configuring Base Drive
      • P Series Letter of Volatility (LOV)
      • P Series Cables - Direct Drive Motor Cable Change
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
P Series Drives - How to Reset Single Turn Absolute Position to Zero (PM-DD example)

Print Friendly and PDF

CONFIRM MOTOR ENCODER PARAMETERS:

Once you get online with the drive you will need to confirm that the ABS Encoder Configuration is set to "Config 2".

Click on the motor icon at the top of the page:

Verify that the ABS. Encoder Configuration is set to "Config 2":

VALIDATE THAT THE DRIVE IS SCALED FOR YOUR DESIRED UNITS

Click on the gear icon at the top of the page:

Reference the following picture:

Validate that the Motor Direction is the way that you want it to be for positive numbers

The above would be for 1 motor revolution (2^20 = 1,048,576 counts per rev) = 360,000   degrees x 10^-3  (thousandths of a degree).

Validate that the Shaft Revolutions is set to 360000. This allows you to program positions in User Units or Degrees. The resolution is 0.001 Degree. Example 181.500 Degrees = 181500 UU

If motor revs and shaft revs are 1, the setting the commanded distance to 1,048,576 would be 1 revolution.

VALIDATE INDEX CONFIGURATION

Click on the gear icon at the top of the page:

Validate that the INDEX CONFIGURATION section on this page looks like the following picture:

The Modulo factor sets the roll over point, so when 360,000 is reached (1rev), the position then rolls over back to 0.

CLEAR OUT ANY PREVIOUS HOME OFFSETS AND SET NEW MACHINE ZERO POSITION

Click on the "Cyclic Monitor" button:

You will be able to monitor the position from here:

Click on the "Homing" icon:

On the Right Hand Side of the screen you should see the following window:

Set the "Homing Method" to 35

Set the "Home Offset" to 0 and Press the Enter Key

Press the "Drive ON" button

Press the "Homing" button

You will see that the position of the motor will change to zero in the monitoring screen:

Press the "Drive OFF" button

Press the "Save to Memory" button to save these changes:

NOTE:  IT IS IMPORTANT NOT TO WAIT FOR THE FOLLOWING MESSAGE BOX TO DISAPPEAR AUTOMATICALLY:

Once the box has disappeared, press the "Software Reset" button or cycle Power on the drive:

Once the drive has reset or cycled power you can see that the position will change:

This is the motor shaft's current position with respect to the Index Pulse of the motor's encoder.

At this point you will want to manually position the motor/load to the Machine Zero Reference point that you desire.

Once you have done this you will look at the "Position Actual Value" under "Cyclic Monitor":

This position is the what we want to use for the Home Offset. We actually want to use the negative value for this number.
You will plug this into the "Home Offset" value:

Press the "Save to Memory" button to save these changes:

NOTE:  IT IS IMPORTANT NOT TO WAIT FOR THE FOLLOWING MESSAGE BOX TO DISAPPEAR AUTOMATICALLY:

Once the box has disappeared, press the "Software Reset" button or cycle Power on the drive:

Once you have done this you will look at the "Position Actual Value" under "Cyclic Monitor" and you will notice that the position now reads 0 or close to 0 (if Modulo is 360,000 for example it may read 359999.
This is your new Machine Zero Reference. All absolute moves will be be referenced to this zero position:

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply