Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • 590+ - Transferring a Configuration to a Drive with a Different Power Level
      • 598/599+ Stack Controller Replacements
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • How do I convert DC590+ Europe part numbers to US part numbers?
      • Speed Regulation with 590+ Drives
      • Troubleshooting a DC brushed motor
      • What are differences between a Regen and Non-Regen 590+?
      • What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
      • Why is every light on the keypad flashing on my 590+?
    • AC890 Series+
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?

Print Friendly and PDF

My 590+ drive is displaying a Missing Pulse alarm on the keypad. What should I do?

What is the missing pulse trip?

This trip is triggered when a pulse(s) is missing from the 6-pulse armature current waveform. It is enabled when the motor loading exceeds 1.5 times the DISCONTINUOUS parameter value.

  • Connect an oscilloscope across the Armature to verify whether there is a missing pulse.
  • Is there a Drive Isolation Transformer for this drive? Is a Line Reactor installed for this drive?  Does the missing pulse only occur with other drives running? As these could be affecting the drive.
  • Has this system been autotuned?
    1. Autotune the system if the drive has not been yet. The autotuned procedure can be found in the manual. Use the manual that corresponds with your drive’s firmware revision.  Make certain the armature does not move during the autotune.
  • Are the SCR connections loose?
    1. Check the SCR connections between the SCR leads and the trigger board.
    2. Insure the SCR bridge connections are not loose.
  • Is the SCR defective?
    1. Check the Gate-Cathode resistance of the SCR. The actual resistance is not important.  However, the resistance of all the other SCRs must be within 10%.
      1. They should tend to be around 8ohms. So 7.2 to 9.2 ohms is normally okay. Anything above or below that is an issue.
    2. Visually check the SCR to make sure it is not damaged. When an SCR faults, it often faults shorted, but occasionally it faults open.
  • Is there a defective pulse transformer on the power board or firing board?
    1. Check the resistance of the pulse transformer winding. The actual resistance is not important.  However, the resistance of all the other windings must be within 10%.
  • Is there a motor short?
    1. Check the motor with a megger to check for insulation and continuity issues.
    2. Use the below document to check the field windings of the motor
  • Is there a feedback on the device?
    1. Check coupling tightness between the motor and the feedback device
    2. Check connections between the feedback device and the feedback card
    3. Check the feedback signal to make sure that is no noise in the system
  • Are you using the speed loop?
    1. Check the gains in the speed loop they may be too high and might need to be adjusted (Note that ripple from the speed loop from either the setpoint or feedback can cause unstable current)

[QuickLink for the 590+ on Parker.com] - Manual, QuickStarts, Product Support, etc

1/5/2018 SV

  • Missing Pulse
  • Alarm
  • 590+
  • Trip
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • ichavarria@corteacero.com.mx
    ichavarria@corteacero.com.mx over 1 year ago

    someone solve this problem? rigth now i have this problem, what happen if i increasse the DISCONTINUOUS parameter?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply