Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample

Print Friendly and PDF

SuperJog screen
Allows you to enable, jog, reset (zero position), set a position & goto that position.
Limits & home aren't set by default in the ACR9000 Configuration Wizard so that a 2axis bench test will work by default
but the homing won't work unless you've a home switch wired and defined limits & home in ACR-View Configuration Wizard (Axis > Fault)

Teach panel

Recipe viewer is shown but need to click Load Recipe first to toggle through recipes.
There's single axis recipes (0pos1 is axis0 position 1, 1pos2 is axis1 position 2, etc) and 2axis recipes (XY0, XY1)
You can load a recipe to view it but then you need to send it to the ACR9000 with Send Recipe.
You can also upload and save to overwrite a recipe, or save as to create a new recipe.

Note the Homing and Distance based moves are controlled through Prog0 and it needs to be running.
After downloading, you can Run from toolbar (play button icon) or from terminal emulator RUN PROG0.
It's set as a PBOOT program and if you cycle power or REBOOT it will be running automatically.
In ACR-View > Status Panels > Common Status panel, program status shown if running or idle.

ACR7000_Xpress_JogTeach.zip

ACR9000_Xpress_JogTeach.zip

Note: ACR7000 series also uses same communications as ACR9000 and the above also works with the new 7900 (ACR7000 controller), 7000 stepper or servo.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply