Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base General - Calculating rotary and electrical power
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base General - Calculating rotary and electrical power
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
  • +Motion and Machine Controllers
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC/DC Industrial Drives
  • -Servo Motors
    • General - Calculating rotary and electrical power
    • MPW Motors - Does the MPW work in salt-rich environments?
    • MPP/MPJ Motors - Feedback data made available to the user when using Hiperface DSL in MPP servo motor (feedback option 6H)
    • BE Motors - Full Specifications
    • BE Motors - BE and SM Encoder Change
    • BE Motors - BE23 Brake Option Length Adder
    • BE Motors - G winding specifications
    • BE Motors - IP Rating for the BE Motors
    • BE Motors - MS, GS, PS & TQ Mating connector - SM & BE motors
    • BE Motors - Replacement of BE motor with Q encoder option
    • BE Motors - Temperature Wires for BE 16 frame motors
    • BE Motors - Wire gauge (AWG) For BE Series Motors with Flying Leads
    • Cables - BE, SM, NeoMetric/J Cable Options
    • Cables - Cable Kits
    • Cables - Drawings for Flying-Lead PS cables
    • Cables - Environmental specs for PS cables
    • Cables - MPM to MPA or MP-FLX or BLOK or SFD Drive Cable Drawings
    • Cables - MS feedback cables for ViX/Aries and Compax3
    • Cables - PS Cable Specifications
    • Cables - PS Connector Kits
    • Cables - PS Connector Specifications
    • Cables - PS Connector Wiring Pinouts
    • Cables - PS Motor Cable Wire Gauge
    • Cables - Replacements for Discontinued Cable Sets
    • Cables - VIDEO: How to find cables for Parker motors?
    • Cables - What are the height dimensions of the Parker Style PS connectors?
    • DX Motors- Servo Wheel weights (discontinued product)
    • EX/EY Motors - EX Cable selections for CE/ATEX and UL models
    • General - Checking Servo Motor Phases
    • General - Customized Servo Motors
    • General - Delta vs Wye phase connections
    • General - EME (Europe) motors crossover to EMN (North America) motors
    • General - EME (Europe) Parker SMB SME SMH MB ME MH motors
    • General - Grades of steel used in servo motor shafts
    • General - Hall Sensors: 60 vs 120degrees
    • General - Industrial servo motor output shaft diameter modifications
    • General - Industrial servo motors in low temperature applications
    • General - Industrial servo motors in vacuum environments
    • General - Linear Motor Sizing
    • General - Linear Servo Motor Parameters
    • General - Magnetic fields and Servo Motors
    • General - Mechanical Time Constants for Servo Motors
    • General - Minimum temperature of the Servo motors
    • General - Motor Connector Pinouts
    • General - Operating Temperatures for Servo Motor Brakes
    • General - Rated Bearing Loads for Compumotor Servos
    • General - Servo Motors: Checking Servo Motor Phases
    • General - SL Magnetic Force.
    • General - Smart Encoder vs Absolute Encoder
    • General - Testing Encoders on Compumotor Servo Motors
    • General - Thermal switch specifications
    • GM Motors - Replacing Bayside GM gearmotors
    • HDX/HDY/HJ Motors - IP Specifications for Hauser HDY, HJ Motors
    • HDX/HDY/HJ Motors - Specifications
    • Kit Motors - Frameless Kit Motors (Inspection Report)
    • Kit Motors - Bayside Brushless Kit (K series) motors FAQs
    • Kit Motors - Frameless Kit Motor windings
    • Kit Motors - Frameless kit motors in extreme environments
    • Kit Motors - How to use Motion Sizer for K series Frameless Kit motor applications
    • Kit Motors - Kit motor cross reference overview
    • Kit Motors - Kit motor mounting best practices
    • Kit Motors - VIDEO: How to Integrate Frameless Kit Motors
    • M Motors - MS & PS Mating connector for the M Series Motors
    • MPM Motors - Converting from older MTS to Current Part Numbers
    • MPM Motors - Encoder Option 1 Software Setup for Vix Drives
    • MPM Motors - IDC B-Series Replacement Options
    • MPM Motors - MaxPlus (MPM) Resolver Option 1 Connection for Vix Drives
    • MPM Motors - MPM Motor Specifications and Performance
    • MPM Motors - MPM Number of Motor Poles
    • MPM Motors - Recommended replacements for MPM72 series: NeoMetric N070
    • MPM Motors - Trap Option: Use Sine as a Drop-In
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (230VAC Encoder & Resolver) to Parker MPP
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (230VAC Hiperface) to Parker MPP
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (460VAC Encoder & Resolver) to Parker MPP
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (460VAC Encoder & Resolver) to Parker MPP (640 & larger)
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (460VAC Hiperface) to Parker MPP
    • MPP/MPJ Motors - Crossover of Allen Bradley Rockwell MPL series motors (460VAC Hiperface) to Parker MPP (640 & larger)
    • MPP/MPJ Motors - Motor Weights for MPP190 and MPP270 frame motors
    • MPP/MPJ Motors - MPP motor right angle PS connector dimensions
    • MPP/MPJ Motors - Replacements for MPP / MPJ servo motors with 3E encoder option
    • MPP/MPJ Motors - Thermistor
    • MPP/MPJ Motors - VIDEO: Parker's MPP Servo Motors
    • MPW Motors - Crossover of Allen-Bradley MPS to MPW Stainless Steel series motors
    • MPW Motors - O-Ring seals for front of MPW Stainless Steel servo motors
    • N/J Motors - Difference between NeoMetric size 70mm and size 34
    • N/J Motors - J series speed/torque curves
    • N/J Motors - MS, PS, & TQ Mating connectors
    • N/J Motors - Pinout for the N092 Motor (MS18-5) Connector?
    • N/J Motors - Replacements for NeoMetric / J series with Q encoder option
    • NM Motors - NM17 NM23 NM34 NM42 Servo Motor Specifications
    • P Motors - P Series Motors and Cables (Specs and Additional Information)
    • Resolver Cable Part Number Change for Servo Motors
    • S Servo Motors (from MTS-Germany)
    • SE Motors - Specifications
    • Servo Cable Selection & Drawings and Motor Pinouts
    • Servo model for Delta phase connected servo motor
    • Servo model for Wye phase connected servo motor
    • Servo Motor Cable Diameters & Bend Radii
    • Servo Motor Cable Part Number Change
    • Servo Motor Hi-Flex Cables
    • Servo Motor Replacement Information
    • Servo Motor Thermal Sensors (BE, SM, MPP, P)
    • Servo Motors: Absolute Encoders & Drive Compatibility
    • ServoMotor Current Units RMS vs Pk of Sine vs Trap
    • SM motor with Q encoder replacements
    • SM Motors - Axial pre load specifications of the SM motors.
    • SM Motors - BE and SM Encoder Change
    • SM Motors - Brake specifications for the SM and N0 motors
    • SM Motors - IP65 option with SM and Neometric motors
    • SM Motors - MS, GS, PS & TQ Mating connector - SM & BE motors
    • SM Motors - Powering the SM and N (Neo) encoders
    • SM Motors - Radial Shaft Runout for Parker Servo Motors
    • SM Motors - SM Flexible Cable Wiring Diagram
    • SM Motors - SM motor cables -TQ , -MS, -GS versions
    • SM Motors - SM Motor Order Code
    • SM Motors - SM motor T shaft option
    • SM Motors - SM Series 23 Connection Diagram
    • SM Motors - SM Series Size 16 Connection Diagram
    • SM Motors - SM speed/torque curves & encoders
    • SM Motors - SM/NeoMetric Encoder Specs
    • SMN Motors - Brake Specifications for SMN Series Motors
    • Standard resolver in MPM and MPP series motors
    • Ultramaster Motor files for MPN
    • Understanding Servo Motor Time Constants
    • Vacuum and Explosion Ratings
    • What are the dimensions of the additional tapped holes in my MPP motor housing?
    • What are the explosive atmosphere certifications for EX_EY motors?
    • What are the SL motor magnet bar weights?
    • What replaces Compumotor 23frame gearmotors?
    • What replaces Compumotor 34frame gearmotors?
    • What replaces Compumotor 92frame gearmotors?
    • What's continuous stall torque vs rated torque vs peak torque?
    • Where Are The Digiplan ML Servo Motor Specifications?
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)

You are currently reviewing an older revision of this page.

  • History View current version

General - Calculating rotary and electrical power

Introduction

The scientific law of conservation of energy dictates that energy cannot be created nor destroyed, but it can be converted. In other words energy that is used in some given situation must come from another source of energy. It cannot come from “thin air.” However, energy comes in many forms and can be exchanged from one form to another (i.e. chemical, thermal, gravitational, among many others).

Likewise, mechanical rotary power given from a motor must be driven by an appropriate amount of electrical power provided by the drive. Like the energy example, rotary power is provided for by the electrical input power, and, also like the energy example, the rotary power cannot exceed the electrical. Therefore, it is important to verify the power throughout the system from power supply all the way to the motor or gearbox output shaft.

Note that this article assumes that the reader has a foundational understanding of Ohm’s Law (V=IR), conservation of energy, and algebraic operations.

Foundations

The foundational power equations are as follows:

Where Pe is electrical power and Pr is rotary power, V is voltage, I is current, τ is torque in Nm, and ω is speed in RPM.

Rotary Power

Mechanical power is a force exerted through a distance over some period of time. The rotational version is torque exerted through some angle over some time period. Therefore, multiplying torque by speed and an additional conversion factor results in mechanical rotary power, Pr.

Electrical Power

Electrical power, Pe, is voltage multiplied by current; however, due to the variable nature of electricity it is commonly not this simple. There are three forms of electrical power that your application could be classified into.

1.) DC power supply

This is the most straightforward form of electricity and calculation is relatively simple. The voltage term in the power equation is simply the DC voltage input value.

Current supplied to the drive is DC current, but the current is processed into a sinusoidal wave to drive the motor. Unfortunately, there are different methods to process that signal, and therefore, this step requires investigating the type of current rating the drive uses. Find the continuous current limit for the drive and whether it is peak-of-sine or RMS. The power equation is in terms of peak-of-sine so if the current rating is in RMS then you will need to multiply by the square root of 2.

Multiply VDC by the rated current in terms of peak-of-sine to find the electrical power that the drive is capable of.

2.a.) AC power supply (in phase)

The governing electrical power equation for AC is more complex because of the ‘alternating’ nature of the current. The most simplistic power formula for alternating current is as follows:

And this equation is related to the graphic below amperage oscillations are in sync with voltage oscillations.

Voltage and current are both defined as RMS, but what if your drive is specified in terms of peak-of-sine? Divide the peak-of-sine value by the square root of 2 to find the equivalent RMS value as shown in the previous section.

2.b.) AC power supply (phase shifted)

Sometimes, however, voltage and current are not synchronized as shown in the previous section. One situation this can occur is when a standard transformer is used to rectify the alternating current brought into a drive. Below is an example of a traditional transformer.

To give some background on transformers, they come in many shapes and sizes but basically use coiled copper to change or ‘transform’ the power signal. Unfortunately, there is a phase shift introduced due to the nature of current flowing through coiled wire and the property of inductance.

When the voltage and amperage are out of phase the available power is reduced by the cosine of the phase shift angle. Therefore, the power equation is extended to the following form:

Note that this only applies if there is a phase shift between voltage and current! If the phases of the voltage and current are aligned (i.e. zero phase shift) then the cosine term goes to 1.

The following plot graphically describes what a phase shift would look like.

Unfortunately, the effect that a phase shift has on a system can only be quantified empirically through experimentation. Prediction of the phase shift is well beyond the level of this article, and as such this topic is mentioned only make the reader aware of its existence and influence on the system.

The plot below compares the instantaneous and average power between the in-phase and out-of-phase condition. One can rather easily see that the phase-shifted average power is less.

Power Balance

We can now look at the efficiency of a system. Recall that the laws of nature require that power out cannot be greater than power in. Since they also dictate that a system cannot be perfectly efficient, there must be some term introduced that accounts for this efficiency loss.

The general equation above accounts for losses in the drive including phase shift, resistive losses in the wiring, and electrical and mechanical losses in the motor. Therefore, the E is not just one number; the total system efficiency is a product of the efficiencies of each component.

Typical efficiency of each component:

  • ηdrive: about 95%
  • ηwires: typically neglected
  • ηmotor: widely variable from 50% to 90% and dependent on the motor's speed, torque, and winding parameters

Therefore, the total available rotary output power is equal to the electrical input power times the total efficiency. Keep in mind that this available output power is a best-case scenario since other small losses have been neglected.

Where to find the efficiency data

Drive and gearbox efficiencies are often published in catalogs and datasheets. Drives are in the realm of 95% while most all planetary gearboxes are above 90%.

Motors have an extensive efficiency range that depends on multiple variables including winding specifications, running speed and torque, and ambient temperature among others. The motor’s performance documentation will sometimes include this.

Phase shift losses will be determined entirely by the electrical components used in the drive’s construction. The amount of phase shift in any given drive can only be quantified empirically through experimentation. Further details of phase shift effects are well beyond the scope of this article.

Extending beyond the motor

Adding gearheads to the equation

Gearheads are commonly attached to motors for many reasons, namely to gain a mechanical advantage or reduce cogging effects. Thankfully, the same power equation that is applicable to motors also applies to gearheads; one just needs to account for the efficiency of the gearhead in addition to all the other components. The power balance equation is extended to the following equation where Pr refers to the gearhead output rather than the motor output:

Calculating current drawn from power supply to drive

Understanding the previous equations allows a rough calculation of the current drawn from the power supply. In the case of a DC power supply:

And in the case of an AC power supply:

Summary

  • Power out of a system can never be more than power into a system.
  • Efficiency of each component must be accounted for to find the maximum power a system can output relative to the power brought in.
  • This can be a great step to take as a sanity check that you have a properly sized drive for the application since all drives have a power output limit. Typically, this limit is seen in the rated amperage limit.
  • Power out of a system can never be more than power into a system.