Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)-
      • PS Series PowerStation will not boot up,
      • Removing the splash screen from the P9 or PS?
      • Weight of my PS-Series PowerStation
      • What replaces my old CTC powerstation that is running Interact?
      • How to get the application off old HMIs running Interact
      • MotionPanel replacement
      • Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.
      • UDP Network traffic when Interact HMI installed
      • Upgrading your Interact HMI - Boot Drive / Storage Warning for P11-xxxxR, P21-xxxxR Model Number format and Models starting with PWR
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.

Print Friendly and PDF

The units with part numbers that follow the pattern of P?-###?? were originally designed and manufactured before there was any such thing as a Compact Flash Card.

The P1 units will have a flush back shell and there is a memory module about 2.25 x 2.25 x .25 inches the may be labeled Model FLH-1004 4M FLASHDISK (4 Meg Flash) This memory module does not have an interface that is compatible with anything other than one of the old P1 units. To upload the information from it requires a working P1 unit. The module can be removed and moved to another unit of the exact same type as it is basically the Hard Drive of the DOS hardware. It contains all of the boot files and MSDOS software as well as the Interact software, applications and utilities.

Later models incorporate the CF Card technology via an adapter module which replaced the molded Flash Drive. This CF card can be used with USB card readers on your Windows PC to copy all of the files into a folder for archival purposes. Be sure to set the explorer to "show hidden files" and uncheck the option to "hide system files" so you get everything that the machine builder put on the card.

CF Card      

P1x-XXX There are 3 manuals available for the different revisions of hardware. Revision numbers were after the dash at the end of the serial number and the manufacture date was also on that label. The revision number of the Manual is independent of the hardware revision number. Compare dates of hardware to release date of the manual revision. Worst case, just look in the files for the one that matches your hardware.

Rev102 04/98 - P1 rev 101 manual in pdf format

Rev102 03/99 - P1 rev 102 manual in pdf format

Rev105 11/99 - P1 rev 105 manual in pdf format

PMP-XXX  is just a P11 that came preloaded with an application that controlled a Parker 6K controller. PMP stands for Parker Motion Panel. There are two versions of the PMP QuickStart and User Guides.

Rev101 - 09/00 PMP rev 101 QuickStart guide in pdf format

Rev102 - 03/03 PMP rev 102 QuickStart guide in pdf format

Rev100 - PMP rev 100 User guide in pdf format

Rev101 - PMP rev 101 User guide in pdf format

P1H-xxx is a Standard P1 hardware with only the PTM module enabled. 1 Guide and 2 Upgrade Guides.

Rev100 - 10/00 - P1H Instruction Sheet in pdf format

Rev100 - 02/01 - Upgrading Module License rev 100 in pdf format.

Rev101 - 04/03 - Upgrading Module License rev 101 in pdf format

P12-x44 is a P1 with Pentium Processor. 1 User Guide

Rev100 - 01/01 - P1 Pentium User guide in pdf format

P1X-PC104 is a PC104 upgrade option that allowed 3rd party PC104 interface cards to be attached.

Rev100 - 05/99 - P1 PC104 Upgrade option Install Guide rev 100 in pdf format

Rev101 - 02/01 - P1 PC104 Upgrade option Install Guide rev 101 in pdf format

All of the 6" display units are replaced by ether the P13 or PA206 whose specs can be found on our current products Dedicated HMI pages.

The 10" version is replaced by the PA210 family whose specs can be found on our current products Dedicated HMI pages.

02/26/2018 dm

  • INTERACT
  • P1
  • PC104
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply