Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How to add images to a visualization in WebVis
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How to add images to a visualization in WebVis
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
  • -Motion and Machine Controllers
    • +ACR Controllers
    • +PAC120
    • +PAC340
    • -PAC320 (Discontinued)
      • +3rd Party Samples
      • +Embedded Xpress
      • +Errors
      • +Hardware
      • +PAM IDE
      • +Programming Tips
      • +Web Visualization
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

How to add images to a visualization in WebVis

Many HMI applications require the use of user-supplied images to represent the machine, display a logo or simply accent the interface to achieve the desired look and feel. WebVis allows you to import your own images into PAM using Image Pools. The procedure outlined below will allow you to import any of the following formats:

  • PNG
  • JPG
  • SVG
  • BMP
  • GIF
  • TIF/TIFF
  • EMF
  • ICO

The most common image formats are PNG, JPG, SVG, BMP and GIF. Please note that animated GIFs will not run their animations in WebVis. Instead, they will appear as static images.

To add an Image Pool to your application and place an image on one of your visualizations, follow these steps:

  1. Add an Image Pool. Right-click on Application, click Add Object and then click Image Pool.

    IMAGE BROKEN -- DCLIFFE
  2. Give the Image Pool a name (the default is fine) and click OK.

    IMAGE BROKEN -- DCLIFFE
  3. Double-click the File name field and then click the ellipsis (...) button.

    IMAGE BROKEN -- DCLIFFE
  4. In the Select Image dialog, you have three options for adding the image to your Image Pool. The default is embed into project, which adds a copy of the image file into your project. This is good for most projects because it means you can move your project to another PC and still have all the images you added. If you have a lot of images, you may want to choose one of the linking options in order to reduce the project's file size. Using linked images is also advantageous for machine builders who want to manage their image resources from a central location and easily make changes across multiple projects.

    Once you know how you want to bring your image into your project, click the ellipsis (...) button.

    IMAGE BROKEN -- DCLIFFE
  5. The image is now part of your Image Pool. It is given an ID in the left-hand column that can be used to attach it to a tool or image element in your WebVis application. You can change this ID by double-clicking on the ID field.

    IMAGE BROKEN -- DCLIFFE
  6. You can add an image to your visualization by dragging an image element from the Toolbox onto the visualization.

    IMAGE BROKEN -- DCLIFFE
  7. Once the image element is added, PAM will automatically prompt you for an image to use. Select your Image Pool from the list view on the left, then select your image from the preview window. Then, click OK.

    IMAGE BROKEN -- DCLIFFE
  8. The image will now appear in your visualization with its default size. You can resize it using the image handles or by editing its size in the image's Properties panel.

    IMAGE BROKEN -- DCLIFFE

Notes:

  • You can change the image associated with an image element by changing its Static ID in the Properties panel.
  • Many different types of tools can use images. Look for a Bitmap info section in the tool's Properties panel.
  • Some tools allow you to change the image shown using a string variable. These tools will have a Bitmap ID variable section in the tool's Properties panel.
  • Not seeing the options in the notes above? Go to the Properties panel and make sure the Expert box is checked.

01MAR2018 DCLIFFE