Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress-
      • Interact Xpress Misc - How to Flashback Compact Flash (CF) Card for Parker HMIs
      • Device Read Error with MicroLogix
      • Flash Player - Parker Remote Browser compatibility issues with the older versions of Xpress
      • Interact Xpress C3 Error History Display
      • INTERACT XPRESS HOW TO ORDER
      • Interact Xpress Manager - Troubleshooting - Ver 4.2 Error Flash Player not installed
      • Interact Xpress Misc - Are all tags written all the time? Where to set this?
      • Interact Xpress Misc - Can I send an Alarm E-mail to more than one person?
      • Interact Xpress Misc - Creating New Projects for older versions of Xpress using Seed Projects in Xpress Manager 4.x
      • Interact Xpress Misc - How can I find out what TCP/UDP ports my software is using?
      • Interact Xpress Misc - How do I get through my router for remote Interact Xpress panel access?
      • Interact Xpress Misc - How to change the sort order for recipes in Xpress?
      • Interact Xpress Misc - Loading Xpress Application on the XPR on bootup
      • Interact Xpress Misc - Test PLC driver connection setup BEFORE downloading to the HMI - If the Development PC can not talk to PLC, the HMI won't ether.
      • Interact Xpress Misc - Updating the Firmware (Xpress version) on the Xpress HMI Hardware
      • Interact Xpress Misc - Updating Xpress Project Versions & Creating Backup Copy
      • Interact Xpress Misc - User Configurable Driver User Guide (UCON)
      • Interact Xpress Misc - What can I do if I don't know the Xpress Admin Password?
      • Interact Xpress Misc - What size Compact Flash card is supported by XPR/XPC?
      • Interact Xpress Misc - Where is the driver documentation and tag format information?
      • Interact Xpress Misc - Which HMI runs Interact Xpress?
      • Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
      • Interact Xpress Misc - XPC2, XPR2 and EPX2 PowerStations no longer include audio hardware (SB975)
      • Interact Xpress Misc - XPR/XPR2 Flashback Utilities
      • Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
      • Interact Xpress Misc - Xpress Flashback for XTA and required Memory Card.
      • Interact Xpress Misc - Xpress Manager Archive
      • Interact Xpress Misc - Xpress Time and Date Tags and how they are related and used to set the HMI system Time and Date
      • Interact Xpress Software - Control Access to Panels and Tools using the Password User Levels in Xpress / Embedded Xpress (PAC)
      • Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
      • Interact Xpress Software - How do I set a value to my device from my Xpress panel only when a button is pressed?
      • Interact Xpress Software - How do I write/read strings between Xpress (XPR) and ACR?
      • Interact Xpress Software - How to switch screens from a PLC
      • Interact Xpress Software - How to wrap text on a tool in Xpress Manager?
      • Interact Xpress Software - Xpress Recipe Naming
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Controller (Global) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Program (Local) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Driver - Manual Creation of Controller (Global) STRING Tags in Xpress Manager
      • INTERACT XPRESS TRAINING - AB CONTROLLOGIX ETHERNET DRIVER - MANUAL CREATION OF PROGRAM (LOCAL) STRING TAGS IN XPRESS MANAGER
      • Interact Xpress Training - Importing Tags into Xpress from Control Logix / Compact Logix
      • Interact Xpress Training - Interact Xpress with Parker-SSD AC890 Drive Products
      • Interact Xpress Training - Tag Rules (Tag Sharing) Examples
      • Interact Xpress Training - Using with Compax3 for Torque Control (Example)
      • Interact Xpress Troubleshooting - Auto E-Mail on Alarm activity not working with Free E-mail servers
      • Interact Xpress Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Interact Xpress Troubleshooting - Fonts unreadable on tools or animations broken after upgrading 2.16 and older Projects to 3.1 or 4.1
      • Interact Xpress Troubleshooting - If losing connection to PLC, turn on Auto-Demotion
      • Interact Xpress Troubleshooting - IOCTL NDIS REBIND ADAPTER error on XT
      • Interact Xpress Troubleshooting - Messages disappear from Multi-State indicator after application closed and re-opened when & is used in message
      • Interact Xpress Troubleshooting - My Xpress projects disappeared after I upgraded my Pre-2.1.6 version to 2.1.6 or higher
      • Interact Xpress Troubleshooting - My Xpress version did not change when I did an upgrade to the latest version on my development PC
      • Interact Xpress Troubleshooting - Not able to add tags in Tag Editor using (New Tag)
      • Interact Xpress Troubleshooting - Step 3 Error when clicking Design in your Xpress Project
      • Interact Xpress Troubleshooting - UCON Floating point values have Commas where the Decimal point should be
      • Interact Xpress Troubleshooting - Workaround for getting flash to work on Android 4.0xxx revs
      • Interact Xpress Troubleshooting - XPR / XPR2 Flash Player error dialog pop-up (long running script....) or screen stops updating.
      • Interact Xpress Troubleshooting - Xpress Manager / Unable to Exit Runtime or Designer running on Windows 10
      • Interact Xpress Troubleshooting - Xpress Manager crashes when importing a JPG
      • Interact Xpress Troubleshooting - Xpress Manager Menus clipped/chopped off. Setting size to Small/Medium/Large does not change the viewable menu.
      • Interact Xpress Troubleshooting - XT replacement panel won't connect over ethernet
      • Modbus Device Compatibility with InteractX and Interact Xpress
      • Parker Remote Browser -- Connect to Xpress HMI at Startup
      • Xpress 4.2 install OCX failed to register and the Xpress Manager "Help - About IXM " shows blank Flash player version.
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button

Print Friendly and PDF

Xpress application with no Exit button makes it impossible to make hardware setting changes.

Sometimes the button is hidden in the application which requires a certain user level before the button appears and is usable. If you don't have any log in buttons and are not able to contact the machine builder then you will need a copy of the Off Line development software.

If you do not have the Xpress Manager software, scroll to the bottom of this topic for an alternative method of breaking the application startup to access the shell.

The development software can be purchased through your Parker distributor, If the version is newer than what is used on the XPR/XPR2/XTA that is OK since older apps can be loaded WITHOUT updating to the current version and changes can be made and saved in the applications original version.

To get access to the Xpress Shell with the least impact and highest degree of safety, you will need the following.

Xpress Off-Line development

PC with Windows XP/Win7/Win10

USB Compact Flash Card Reader that works with your PC and can see the Compact Flash (CF) card from the XPR/XPR2 when inserted or the SD card from the XTA.

If you open Xpress after the Card is inserted and showing up as a Removable media drive letter, it will show up in the "Remote Machines" Window. If you have Xpress open when the card is inserted, let the PC find it and assign the drive letter then Hit the "Refresh" button or Right Click in the white space of the "Remote Machines" window and do a refresh. The drive letter will show up and you can just click on it to get it highlighted and then the arrow that points to the "Local Projects" window and it will upload the application from the CF card to your PC.

Open the application by double clicking on it in the "Local Projects" screen so it opens the one on your PC.

On the first screen under "User Admin" you will make a change in "Security Options" to change the "Local Startup User" to Admin. Applications with Admin as the local startup user will ALWAYS stop at the Xpress Shell when booting which is where you need to be to make hardware level settings changes.

Make sure to take note of the user it is currently set to since we need that so we can change it back after the changes are made. Changing it back will be done right on the unit and will not require going through the development software again.

Click OK after changing the Local Startup User.

Get back to the main Xpress Shell screen.

Now with the changed application highlighted on the left in "Local Projects" and the Drive letter highlighted the "Remote Machines" hit the arrow goes from Local to Remote.

 

Put the card back in the XPR/XPR2/XTA and when it boots it will stop at the Shell.

After making the changes you needed, Go into the Security right on the hardware and set it back to the original user and after saving change, reboot and it will automatically go into run again.

Alternate method (intentionally breaking the application to prevent the unit from getting past the Shell)

If you DO NOT have Xpress Manager there is another less structured way to force the unit to boot to the Xpress Shell on the XPR/XPR2 and XT (The XTA uses an SD card behind the plate with 4 screws on the back of the XTA hardware)

WARNING: Deleting files or folders that are not specifically referenced below WILL cause the unit to no longer boot. If you are not comfortable manipulating files directly in Windows File Explorer, DO NOT attempt this work around for not having a way to get to the Shell programmed into the application. Deleting/moving/renaming the wrong files could result in having to use the Flashback to return it to factory state and Xpress Manager and a backup of the project to recover. 

This requires you have a CF Card reader for the XPR/XPR2 or an SD Card reader if it is for the XTA HMI hardware.

Using Windows File Explorer, Browse the card and you should see something like this.

The Project Folder contains the application that the machine builder created in Xpress Manager.

RENAME the Project folder Project1 (Do not delete or change any other files or folders.

Return the CF/SD card to the HMI and power up the unit. When it does not find the Project Folder, it will create a new empty folder and stop at the Shell with an error that the project contains no screens.

Run the calibration or make the other changes needed.

Power off the unit and take the CF/SD card back to the PC with the card reader. You will now see both a Project (new one created by Xpress when not found) and the Project1 folder that we renamed earlier.

Delete the folder named PROJECT that was just created.

Rename the Project1 folder back to Project.

Put the CF/SD card back in the HMI and power up. It will now go back into run mode as it always has using the calibration or other changes.

Renaming and deleting folders carries a risk of making the card unbootable if the card is removed from the reader without making sure it is done writing.

Windows/Card Reader issues can also effect the card negatively and this should be attempted as a last resort if you do not have Xpress Manager.

edited dom 02/20/2019

edited dom 11/19/2020

  • Xpress
  • Time
  • XPR
  • IP Addrress
  • XT
  • Autorun
  • XTA
  • Date
  • Xpress Shell
  • XPR2
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply