Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
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
  • +Motion and Machine Controllers
  • +General Technology Information
  • +Virtual Engineer
  • -Visualization and Human Machine Interface (HMI)
    • +General Communications Driver
    • +Interact (Legacy)
    • +InteractX
    • -Interact Xpress
      • Interact Xpress Misc - How to Flashback Compact Flash (CF) Card for Parker HMIs
      • Flash Player - Parker Remote Browser compatibility issues with the older versions of Xpress
      • Interact Xpress C3 Error History Display
      • INTERACT XPRESS HOW TO ORDER
      • Interact Xpress Manager - Troubleshooting - Ver 4.2 Error Flash Player not installed
      • Interact Xpress Misc - Are all tags written all the time? Where to set this?
      • Interact Xpress Misc - Can I send an Alarm E-mail to more than one person?
      • Interact Xpress Misc - Creating New Projects for older versions of Xpress using Seed Projects in Xpress Manager 4.x
      • Interact Xpress Misc - How can I find out what TCP/UDP ports my software is using?
      • Interact Xpress Misc - How do I get through my router for remote Interact Xpress panel access?
      • Interact Xpress Misc - How to change the sort order for recipes in Xpress?
      • Interact Xpress Misc - Loading Xpress Application on the XPR on bootup
      • Interact Xpress Misc - Test PLC driver connection setup BEFORE downloading to the HMI - If the Development PC can not talk to PLC, the HMI won't ether.
      • Interact Xpress Misc - Updating the Firmware (Xpress version) on the Xpress HMI Hardware
      • Interact Xpress Misc - Updating Xpress Project Versions & Creating Backup Copy
      • Interact Xpress Misc - User Configurable Driver User Guide (UCON)
      • Interact Xpress Misc - What can I do if I don't know the Xpress Admin Password?
      • Interact Xpress Misc - What size Compact Flash card is supported by XPR/XPC?
      • Interact Xpress Misc - Where is the driver documentation and tag format information?
      • Interact Xpress Misc - Which HMI runs Interact Xpress?
      • Interact Xpress Misc - Which Xpress Version works with my? XPR / XPR2 / XT
      • Interact Xpress Misc - XPC2, XPR2 and EPX2 PowerStations no longer include audio hardware (SB975)
      • Interact Xpress Misc - XPR/XPR2 Flashback Utilities
      • Interact Xpress Misc - XPR/XPR2/XTA Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
      • Interact Xpress Misc - Xpress Flashback for XTA and required Memory Card.
      • Interact Xpress Misc - Xpress Manager Archive
      • Interact Xpress Misc - Xpress Time and Date Tags and how they are related and used to set the HMI system Time and Date
      • Interact Xpress Software - Control Access to Panels and Tools using the Password User Levels in Xpress / Embedded Xpress (PAC)
      • Interact Xpress Software - How do I control the Lens States for an Indicator tool in Interact Xpress?
      • Interact Xpress Software - How do I set a value to my device from my Xpress panel only when a button is pressed?
      • Interact Xpress Software - How do I write/read strings between Xpress (XPR) and ACR?
      • Interact Xpress Software - How to switch screens from a PLC
      • Interact Xpress Software - How to wrap text on a tool in Xpress Manager?
      • Interact Xpress Software - Xpress Recipe Naming
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Controller (Global) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Communication Driver - Manual Creation of Program (Local) Atomic Tags in Xpress Manager
      • Interact Xpress Training - AB ControlLogix Ethernet Driver - Manual Creation of Controller (Global) STRING Tags in Xpress Manager
      • INTERACT XPRESS TRAINING - AB CONTROLLOGIX ETHERNET DRIVER - MANUAL CREATION OF PROGRAM (LOCAL) STRING TAGS IN XPRESS MANAGER
      • Interact Xpress Training - Importing Tags into Xpress from Control Logix / Compact Logix
      • Interact Xpress Training - Interact Xpress with Parker-SSD AC890 Drive Products
      • Interact Xpress Training - Tag Rules (Tag Sharing) Examples
      • Interact Xpress Training - Using with Compax3 for Torque Control (Example)
      • Interact Xpress Troubleshooting - Auto E-Mail on Alarm activity not working with Free E-mail servers
      • Interact Xpress Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Interact Xpress Troubleshooting - Fonts unreadable on tools or animations broken after upgrading 2.16 and older Projects to 3.1 or 4.1
      • Interact Xpress Troubleshooting - If losing connection to PLC, turn on Auto-Demotion
      • Interact Xpress Troubleshooting - Messages disappear from Multi-State indicator after application closed and re-opened when & is used in message
      • Interact Xpress Troubleshooting - My Xpress projects disappeared after I upgraded my Pre-2.1.6 version to 2.1.6 or higher
      • Interact Xpress Troubleshooting - My Xpress version did not change when I did an upgrade to the latest version on my development PC
      • Interact Xpress Troubleshooting - Not able to add tags in Tag Editor using (New Tag)
      • Interact Xpress Troubleshooting - Step 3 Error when clicking Design in your Xpress Project
      • Interact Xpress Troubleshooting - UCON Floating point values have Commas where the Decimal point should be
      • Interact Xpress Troubleshooting - Workaround for getting flash to work on Android 4.0xxx revs
      • Interact Xpress Troubleshooting - XPR / XPR2 Flash Player error dialog pop-up (long running script....) or screen stops updating.
      • Interact Xpress Troubleshooting - Xpress Manager / Unable to Exit Runtime or Designer running on Windows 10
      • Interact Xpress Troubleshooting - Xpress Manager crashes when importing a JPG
      • Interact Xpress Troubleshooting - Xpress Manager Menus clipped/chopped off. Setting size to Small/Medium/Large does not change the viewable menu.
      • Interact Xpress Troubleshooting - XT replacement panel won't connect over ethernet
      • Parker Remote Browser -- Connect to Xpress HMI at Startup
      • Xpress 4.2 install OCX failed to register and the Xpress Manager "Help - About IXM " shows blank Flash player version.
    • +IX / PCA
    • +IPX / IPC (Discontinued)
    • +PHM / PM1 Industrial Monitors (Discontinued)
    • +PA / PS / P1-P9 (DOS-based Interact HMI)
    • +PX / HPX InteractX HMIs (Discontinued)
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Which Xpress Version works with my? XPR / XPR2 / XT

With the release of Xpress 4.x to support the new XT Widescreen format displays, there are now version restrictions based on the hardware for which you are developing or editing applications.

The XT (Widescreen) Requires Xpress 4.0 and higher. The Compact Flash memory cards that worked in the XPR/XPR2 are not compatible with the XT. The XT uses SD memory cards and requires a newer version of Embedded Windows.

The XPR/XPR2 requires Xpress 3.x and lower. Applications created and or upgraded to 4.x are not compatible with the XPR/XPR2

When opening an existing application, Xpress will ask if you want to upgrade if it is older than the version you are using to edit the files. As long as you reply NO to upgrading, the editor will open in a compatibility mode that can make changes to the old application and save changes that will work on the old units.

If you say YES to the upgrade question, it will give you a range of available versions to use.

IMPORTANT - Once upgraded, it is not possible to "Down Rev" an application. Make copies of original projects and keep the originals as backups. Upgrading goes up but never down. Downloading an older version application from your PC than the HMI has will be corrected by the HMI after the download. The first time it goes into run mode, it will take a while as it upgrades the application to the version it has running on it. If you upload the application back from the unit after it has run, the application will now be at the higher rev level of the HMI and not necessarily compatible with your development software any longer.

Xpress 4.x can not build a new application from scratch for old versions. If you need to support older versions and create applications from scratch, keep a old version application to use as a starter app. Make a copy of the starter app and then when opening it, just say no to upgrading and the editor will open in the older version mode and save your project in the old version format.

edited dom 02/13/2019