Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Sample code for PACIO-442-02 and PACIO-441-02 analog modules
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Sample code for PACIO-442-02 and PACIO-441-02 analog modules
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)-
      • 3rd Party Samples+
      • Embedded Xpress+
      • Errors+
      • Hardware+
      • PAM IDE+
      • Programming Tips+
      • Web Visualization+
      • Quick Start and Online Training Videos
      • Adding New Devices
      • Auto Addressing enabled by default
      • Cam and Gear Program Sample & Video
      • Common PACIO Troubleshooting Tips
      • Compax3 Linear servo motor settings with PAC
      • Default IP Address 192.168.10.50 subnet 255.255.0.0 (X2 port)
      • Reading G Code from a file to develop a CNC machine
      • Error: Red triangle on EtherCAT axes/devices when ModBus or ProfiNet connects
      • FTP support
      • How can I send ASCII strings to or from the PAC?
      • How do I configure and gear to the PACIO-454-01 Module?
      • How do I upgrade a Parker Automation Manager (PAM) project from 1.3.0 to 1.4.0?
      • How do I use variables in G code?
      • How to Add ModbusTCP to PAC project (PAC as ModbusTCP slave)
      • How to Set and Get Time / Date / Time Zone Pre-1.4
      • How to Update Devices and their Descriptor files
      • How to Update PAC project without Parker Automation Manager software?
      • How to Update a PAC Firmware? Flashback instructions
      • How to Upload a Program?
      • How to Use the InteractX OPC Quick Client with the PAC
      • How to set up EtherNet/IP Communications with an Allen Bradley PLC
      • How to set Scaling for Parker Mechanics
      • How to use the Outputs on the Compax3-I31 or P series (EtherCAT)
      • IO settings for EtherCAT_Master: How to see IO update while in Stop
      • Log Data to a File
      • Minimum Internet Explorer version for Xpress and Visualization options
      • PAC CNC & Multi-Axis Capabilities, Samples & Video demos
      • PAC CNC visualization
      • PAC System Time Access and Edits
      • PAC Web Visualization with Internet Explorer: missing browser feature HTML5-Canvas Webvisu
      • PAC with .Net or LabView or InteractX: Using OPC DA Server
      • PAC with Modbus: What addresses for tags?
      • Reading Torque from Pseries drive
      • Remanent Variables: Retain vs Persistent Retain
      • Retentive Memory details
      • SDO Read / Write PAC to/from Compax3 I31
      • SMC_ERROR.SMC_FB_WASNT_CALLED_DURING_MOTION
      • Sample Continuous Function Chart CFC Program: time based counter
      • Sample Continuous Function Chart CFC Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Basic Motion (Power, Home, Cycle)
      • Sample Ladder Logic LD Program: Time based counter
      • Sample SFC Program: time based counter
      • Sample Stuctured Text ST Program: Time Based Counter
      • Sample Structured Text ST Program: Basic Motion (Power, Home, Cycle)
      • Single Axis Sample Program with Visualization
      • Two Axis Sample Program with Visualization
      • Using the PAC as a Modbus TCP Master Device
      • Using the PAC as a Modbus TCP Slave Device
      • VIDEO: Run an AC30V an AC Induction motor via EtherCAT with a PAC
      • VIDEO: PAC with Compax3 EtherCAT part 1: EtherCAT connections & Device Selection
      • VIDEO: PAC with Compax3 EtherCAT part 2: Complete Configuration
      • VIDEO: PAC with Compax3 EtherCAT part 3: Setting EtherCAT Master and DS402 scaling
      • VIDEO: PAC with Compax3 EtherCAT part 4: Download & Test in C3 ServoManager
      • Video: Parker's PAC, the Automation Controller Based on IEC61131-3
      • What's the 16# in the axis scaling default of 16#10000?
      • Working with recipes in the PAC
      • Does the PAC have a first scan flag?
      • Error when switching Active Application
      • Using tappets during cam motion
      • WebVisualization not working in PAC terminal (PTA)
      • Can I open an edit and download a PAM 1.3.0 project using PAM 1.4.0?
      • Does PAC act as a OPC-UA server or client, or both?
      • How do I upgrade the PAC from OPC-DA to OPC-UA?
      • How do I use OPC-UA with the PAC?
      • PACIO-441-01 analog current input module
      • Sample code for PACIO-442-02 and PACIO-441-02 analog modules
      • What ports get used with PAC Ethernet connections?
      • C0032: Cannot convert type 'Unknown type: 'ADR(Device.Application.PLC_PRG.x)' to type 'POINTER TO BOOL'
      • CSV Reader Library for the PAC
      • Do I have to upgrade my PAC 1.3.0 Firmware to work with a PAM 1.4.0 project?
      • eCL Homing notes with PAC via EtherCAT
      • EtherCAT communication between the PAC and AC30 drive
      • How to add images to a visualization in WebVis
      • How to reset the EtherCAT bus
      • PAC Terminal Discontinued - PTA, PTI, PTL
      • Parker Tap Adapter for EoE communications
      • User Management in the Parker Automation Controller
      • Using MC_TouchProbe with Compax3 Series Drives
      • Using MC_TouchProbe with P Series Drives
      • Webvis toolbox missing tabs (Codesys calls them tags) - Added alarms but no Alarms Display tool in toolbox.
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Sample code for PACIO-442-02 and PACIO-441-02 analog modules

Print Friendly and PDF

Example of setting an analog output module PACIO-442-02 and analog input module PACIO-441-02

Note:  Analog output module requires 24volts connected at the bottom. Analog input module does not. If you connect pins0 together between the 2 modules and then also pins1 together on the 2 modules, the voltage will continuously cycle from 0 to 10volts

Select the project that matches your version of Parker Automation Manager:

PAM1.4: Simple_Gearing_to_PACIO454_Encoder_PAM1.4

PAM1.2: Simple_Gearing_to_PACIO454_Encoder_PAM1.2

1NOV18 - JD - update

  • analog
  • PACIO
  • modules
  • 442
  • 441
  • sample
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply